SLAAEH0 November 2023 AFE781H1 , AFE782H1 , AFE881H1 , AFE882H1 , DAC161P997 , DAC161S997 , DAC7750 , DAC7760 , DAC8740H , DAC8741H , DAC8742H , DAC8750 , DAC8760 , DAC8771 , DAC8775
The HART protocol follows the seven-layer Open Systems Interconnection (OSI) protocol model. The OSI model describes seven layers that computer systems use to communicate over a network. Figure 2-1 shows a comparison between the OSI protocol model and the HART protocol.
Of the seven layers of the OSI model, the HART protocol uses three layers to describe network communication.
At the bottom, there is a HART Physical Layer. This is the FSK format for the HART transmission based on the Bell 202 standard. This signal sends data at 1200 baud and is superimposed on the 4-mA to 20-mA analog measurement signal.
Next, the HART Data Link Layer (DLL) defines the communication format and timing rules between the host and the transmitter device. There can be two different hosts on a bus, and in multi-drop mode, there can be as many as 15 devices (HART versions 3 to 5) or 62 devices (HART version 6 or later) connected in parallel.
Finally, there is an Application Layer that has some human or computer interaction that define commands, responses, and data formats that are used in the protocol. As previously mentioned, commands are broken up into several categories for the application layer. These commands are the universal commands, the common-practice commands, and device-specific commands.
Each of the layers use tests to verify different rules in the HART protocol. Testing for HART registration is divided into the three layers, covering the physical layer, the data link layer, and the application layer commands.