SLAAEJ0 November   2023 AM625 , MSPM0L1306

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 SPI Transaction Dataflow
    2. 1.2 AM62x Processor
    3. 1.3 MSPM0L130x Microcontroller
  5. 2Hardware Setup
    1. 2.1 A53 Core Hardware Setup
    2. 2.2 M4F Core Hardware Setup
  6. 3Software Setup
    1. 3.1 Cloning the Beyond SDK GitHub Repository
    2. 3.2 SK-AM62x Software Setup
      1. 3.2.1 A53 Core
      2. 3.2.2 M4F Core
    3. 3.3 LP-MSPM0L130x Software Setup
  7. 4Steps for Execution
    1. 4.1 Run Project on LP-MSPM0L130x
    2. 4.2 Run Project on SK-AM62x
      1. 4.2.1 A53 Core
      2. 4.2.2 M4F Core
  8. 5Results
    1. 5.1 Single Byte Single Channel
    2. 5.2 Single Byte Multi Channel
    3. 5.3 Multi Byte Single Channel
    4. 5.4 Multi Byte Multi Channel
  9. 6Summary
  10. 7References

Cloning the Beyond SDK GitHub Repository

  • Beyond SDK is a GitHub repository that contains some of the files needed for this experiment

  • Find the files in Beyond-SDK/am62x/MSPM0-ADC-RTC-Attach/MSPM0-ADC-Attach-SPI

  • Select one of the folders depending on the application (x_Byte_x_Channel_SPI)

  • In Controller, the A53 Core folder contains the C file and the M4 Core contains a CCS project

  • In Peripheral, there is a CCS project for the MSPM0

  • Here is how to clone the GitHub repository:

HOST$ mkdir <Beyond-SDK-installation-path>
HOST$ cd <Beyond-SDK-installation-path>
HOST$ git clone https://github.com/TexasInstruments/Beyond-SDK.git