SLAU550AB January   2014  – September 2022 MSP430FR2032 , MSP430FR2033 , MSP430FR2110 , MSP430FR2111 , MSP430FR2153 , MSP430FR2155 , MSP430FR2310 , MSP430FR2311 , MSP430FR2353 , MSP430FR2355 , MSP430FR2433 , MSP430FR2532 , MSP430FR2533 , MSP430FR2632 , MSP430FR2633 , MSP430FR4131 , MSP430FR4132 , MSP430FR4133 , MSP430FR5041 , MSP430FR5043 , MSP430FR50431 , MSP430FR5847 , MSP430FR58471 , MSP430FR5848 , MSP430FR5849 , MSP430FR5857 , MSP430FR5858 , MSP430FR5859 , MSP430FR5867 , MSP430FR58671 , MSP430FR5868 , MSP430FR5869 , MSP430FR5887 , MSP430FR5888 , MSP430FR5889 , MSP430FR58891 , MSP430FR5947 , MSP430FR59471 , MSP430FR5948 , MSP430FR5949 , MSP430FR5957 , MSP430FR5958 , MSP430FR5959 , MSP430FR5967 , MSP430FR5968 , MSP430FR5969 , MSP430FR5969-SP , MSP430FR59691 , MSP430FR5986 , MSP430FR5987 , MSP430FR5988 , MSP430FR5989 , MSP430FR5989-EP , MSP430FR59891 , MSP430FR6041 , MSP430FR6043 , MSP430FR60431 , MSP430FR6877 , MSP430FR6879 , MSP430FR68791 , MSP430FR6887 , MSP430FR6888 , MSP430FR6889 , MSP430FR68891 , MSP430FR6927 , MSP430FR69271 , MSP430FR6928 , MSP430FR6972 , MSP430FR6977 , MSP430FR6979 , MSP430FR69791 , MSP430FR6987 , MSP430FR6988 , MSP430FR6989 , MSP430FR69891

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
    1. 1.1 BSL Limitations
    2. 1.2 Other Useful Documentation
  4. 2Overview of BSL Features
  5. 3BSL Architecture
    1. 3.1 Communication Interface
      1. 3.1.1 UART BSL
      2. 3.1.2 I2C BSL
    2. 3.2 BSL Memory
      1. 3.2.1 BSL Memory Layout
      2. 3.2.2 BSL Z-Area
      3. 3.2.3 BSL Memory Consideration
    3. 3.3 BSL Invocation
      1. 3.3.1 Software BSL Invocation
        1. 3.3.1.1 Starting the BSL From an External Software Application
        2. 3.3.1.2 BSL Action
          1. 3.3.1.2.1 BSL Action Function 2
      2. 3.3.2 Hardware BSL Invocation
        1. 3.3.2.1 Factors That Prevent Hardware BSL Invocation
      3. 3.3.3 Blank Device Detection
    4. 3.4 BSL Time-out Feature
    5. 3.5 BSL Version Number
    6. 3.6 BSL (User) Configuration
      1. 3.6.1 Configuring the BSL
        1. 3.6.1.1 Example of BSL User Configuration
        2. 3.6.1.2 Implement BSL Configuration in Application Code
  6. 4BSL Protocol
    1. 4.1 BSL Data Packet
      1. 4.1.1 UART Peripheral Interface Wrapper
      2. 4.1.2 I2C Peripheral Interface Wrapper
      3. 4.1.3 BSL Acknowledgment
      4. 4.1.4 BSL Core Response and BSL Core Message
      5. 4.1.5 BSL Core Commands
        1. 4.1.5.1 RX Data Block
        2. 4.1.5.2 RX Password
        3. 4.1.5.3 Mass Erase
        4. 4.1.5.4 CRC Check
        5. 4.1.5.5 Load PC
        6. 4.1.5.6 TX Data Block
        7. 4.1.5.7 TX BSL Version
        8. 4.1.5.8 RX Data Block Fast
        9. 4.1.5.9 Change Baud Rate
    2. 4.2 BSL Security
      1. 4.2.1 Protected Commands
      2. 4.2.2 RAM Erase
      3. 4.2.3 BSL Entry
  7. 5Common BSL Use Cases
    1. 5.1 Overview and Flow Chart
    2. 5.2 Establish a Connection
    3. 5.3 Erase the Device
    4. 5.4 Download the Application
    5. 5.5 Verify the Application
    6. 5.6 Run the Application
  8. 6Customize the BSL
  9. 7Bootloader Versions
    1. 7.1 FR2xx BSL Versions
    2. 7.2 FR4xx BSL Versions
    3. 7.3 FR57xx BSL Versions
    4. 7.4 FR58xx and FR59xx BSL Versions
    5. 7.5 FR6xx BSL Versions
  10. 8Revision History

Implement BSL Configuration in Application Code

The linker command file for the FR235x and FR215x MCUs has the following sections:

  • .bslconfigsignature
  • .bslconfig
  • .bsli2caddress

In the application code, define the following configuration values:

#define BSL_CONFIG_SIGNATURE                   (0x695A) // BSL Configuration Signature
#define BSL_CONFIG_PASSWORD                    (0x5A00) // BSL User's Configuration Signature
#define BSL_CONFIG_TINY_RAM_ERASED_BY_INIT     (0x0008) // Tiny RAM is erased during BSL invocation
#define BSL_CONFIG_TINY_RAM_NOT_ERASED_BY_INIT (0x0000) // (Default) Tiny RAM is not erased during BSL invocation
#define BSL_CONFIG_RAM_ERASED_BY_INIT          (0x0000) // RAM is erased during BSL invocation
#define BSL_CONFIG_RAM_NOT_ERASED_BY_INIT      (0x0004) // (Default) RAM is not erased during BSL invocation
#define BSL_CONFIG_INTERFACE_UART_I2C          (0x0000) // Enable UART and I2C
#define BSL_CONFIG_INTERFACE_UART_ONLY         (0x0001) // Enable UART
#define BSL_CONFIG_INTERFACE_I2C_ONLY          (0x0002) // Enable I2C
#define BSL_CONFIG_INTERFACE_DEFAULT           (0x0003) // (Default / Reserved) Enable UART and I2C
#define BSL_I2C_ADDRESS_7BIT                   (0x60)   // Customized I2C Address

Apply the intended configuration values to the BSL configuration section:

#pragma RETAIN(bslConfigurationSignature)
#pragma DATA_SECTION(bslConfigurationSignature, ".bslconfigsignature")
const uint16_t bslConfigurationSignature = BSL_CONFIG_SIGNATURE;
#pragma RETAIN(bslConfig)
#pragma DATA_SECTION(bslConfig, ".bslconfig")
const uint16_t bslConfig = (BSL_CONFIG_PASSWORD | BSL_CONFIG_INTERFACE_UART_ONLY) ;
#pragma RETAIN(bslI2Caddr)
#pragma DATA_SECTION(bslI2Caddr, ".bsli2caddress")
const uint16_t bslI2Caddr = (0xFF00 | BSL_I2C_ADDRESS_7BIT) ;