SLAU847D October 2022 – May 2024 MSPM0L1105 , MSPM0L1106 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2228 , MSPM0L2228-Q1
The input select bits TIMx.IFCTL_xy[0/1].ISEL select the input source to the filter input as the corresponding CCP input, CCP0 for cross-triggering across CC blocks, an external trigger, XOR (used in Hall input mode), event subscribers, or comparator inputs.
Input selection (TIMx.IFCTL_xy[0/1].ISEL) | Source |
---|---|
0h | TIMx CCP of the corresponding capture compare unit |
1h | Input pair CCPx of the capture compare unit. [CCP0/CCP1, CCP2/CCP3] |
2h | TIMx CCP0 |
3h | Cross trigger signal |
4h | XOR of CCP inputs. Used in Hall input mode. See Section 23.2.3.1.4 |
5h | Subscriber event 0 (FSUB0). See Section 23.2.9.2 |
6h | Subscriber event 1 (FSUB1). See Section 23.2.9.2 |
7h | COMP0_OUT (devices with comparator only) |
8h | COMP1_OUT (devices with comparator only) |
9h | COMP2_OUT (devices with comparator only) |