SLAU847D October 2022 – May 2024 MSPM0L1105 , MSPM0L1106 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2228 , MSPM0L2228-Q1
The brownout reset (BOR) supervisor monitors the external supply (VDD) and asserts or de-asserts a BOR violation to SYSCTL. The primary responsibility of the BOR circuit is to make sure that the external supply is maintained high enough to enable correct operation of internal circuits, including the core regulator. The BOR threshold reference is derived from the internal bandgap circuit. The threshold is programmable and is always higher than the POR threshold. During cold start, after VDD passes the POR+ threshold, the bandgap reference and BOR circuit are started. The device is then held in a BOR state until VDD passes the BOR0+ threshold. When VDD passes BOR0+, the BOR supervisor releases the device to continue the boot process, and the PMU is started.
There are four selectable BOR threshold levels (BOR0-BOR3). During startup, the BOR threshold is always BOR0 (the lowest value) to make sure that the device starts at the specified VDD minimum (1.62V). After boot, software can optionally re-configure the BOR circuit to use a different (higher) threshold level (BOR1-BOR3).
When the BOR threshold is BOR0, a BOR0- violation always generates a BOR- violation signal to SYSCTL, generating a BOR level reset. When the BOR threshold is re-configured to BOR1, BOR2, or BOR3, the BOR circuit generates a SYSCTL interrupt rather than asserting the BOR- violation. This can be used to give the application an indication that the supply has dropped below a certain level without causing a reset.
To change the BOR level from the default (BOR0), first select the desired value in the LEVEL field of the BORTHRESHOLD register in SYSCTL. Then, activate the threshold set in the LEVEL field by setting the GO bit in the BORCLRCMD register. The change can be validated by testing the BORCURTHRESOLD field in the SYSSTATUS register, which returns a value corresponding to the currently active BOR threshold. The BOR threshold change takes approximately 15µs to complete, during which time the BOR circuit is blind to changes in the supply.
If the BOR is in interrupt mode (a threshold level of BOR1-BOR3), and the supply drops below the corresponding BORx- level, an interrupt is generated and the BOR circuit automatically switches the BOR threshold level to BOR0 to make sure that a BOR- violation is asserted if VDD drops below BOR0-. Application software can set the BOR level back to the level specified in the LEVEL field of the BORTHRESHOLD register by setting the GO bit again in the BORCLRCMD register.
The BOR supervisor is active in RUN, SLEEP, STOP, and STANDBY modes but is disabled automatically in SHUTDOWN mode.