SLAU847D October 2022 – May 2024 MSPM0L1105 , MSPM0L1106 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2228 , MSPM0L2228-Q1
The low-frequency crystal oscillator (LFXT) is an ultra-low-power crystal oscillator that supports a standard 32.768kHz watch crystal.
To use the LFXT, place a watch crystal between the LFXIN and LFXOUT pins. Place loading capacitors on both pins to circuit ground (VSS). Size the crystal load capacitors according to the specifications of the crystal being used. A variety of crystal types are supported through a programmable drive mechanism that allows for balancing drive current with the required drive strength for a particular crystal.
The LFXT pins LFXIN and LFXOUT are shared with digital IO functions. To use the LFXT, first configure the IOMUX to support LFXT functionality on the LFXIN and LFXOUT pins. Configure IOMUX to disable any digital IO functionality on the LFXIN and LFXOUT pins. The LFXT defaults to the highest drive strength (LFCLKCFG.XT1DRIVE == 0x03 in SYSCTL), which is recommended for fast reliable start-up of the oscillator. If a crystal with ultra-low capacitance (<3pF) is used, power consumption of the LFXT can be lowered further by setting the LOWCAP bit LFCLKCFG (LOWCAP is cleared by default for compatibility with most crystals).
After completing configuration, start the LFXT by setting the STARTLFXT bit in the LFXTCTL register in SYSCTL. When the oscillator has started successfully, the LFXT startup monitor sets the LFXTGOOD bit in the CLKSTATUS register in SYSCTL. Crystal drive strength can then be reduced to conserve power, if desired. Once STARTLFXT is set by the application software, the internal LFOSC is disabled to conserve power while the LFXT starts in anticipation of LFCLK moving to the LFXT.
To switch the LFCLK tree to use LFXT as the 32kHz clock source rather than LFOSC, set the SETUSELFXT bit in the LFXTCTL register, and SYSCTL permanently switches the LFCLK source to LFXT.
After the LFXT is enabled, the internal LFOSC is permanently disabled. LFOSC cannot be re-enabled and LFCLK thus cannot be switched back to LFOSC other than by executing a BOOTRST.