SLOA332A July   2023  – September 2024 LMV821-N , LMV831 , OPA2991 , OPA345 , OPA376 , OPA376-Q1 , OPA377 , OPA377-Q1 , OPA4991 , OPA991 , TL074 , TLV376 , TLV9001 , TLV9002 , TS321

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Slew Rate Definition
    1. 1.1 Virtual Ground and Slew Rate
  5. Bipolar Op Amp Slew Rate Example
  6. CMOS Op Amp Slew Rate Example
    1. 3.1 Slew Boost Example 1
    2. 3.2 Slew Boost Example 2
    3. 3.3 Slew Boost Summary
  7. Four Methods to Determine Boost or No Boost Using the Data Sheet
    1. 4.1 Method 1: Compare Slew Rate Versus Gain Bandwidth
    2. 4.2 Method 2: Compare Quiescent Current Versus Similar SR Devices
    3. 4.3 Method 3: Evaluate Large Signal Response
    4. 4.4 Method 4: Evaluate Small Signal Response
  8. Slew Rate Dependencies on Circuit Signal Levels and Op Amp Gain Set by Feedback Network
  9. How Much Output Slew Rate is Needed to Support a Sine Wave or Other Non-step Inputs
  10. Stability Also Plays a Role in Observed Slew Rate
  11. Summary
  12. References
  13. 10Revision History

Method 4: Evaluate Small Signal Response

The fourth method is to evaluate the SR in small input signal charts. Use the chart with the smallest input signal and highest noise gain. It can be necessary to zoom in to accurately measure the waveform relative to division scaling to get the initial slew rate after any internal capacitive-forward coupling. The time division of the TLV9001 waveform is too long, making the rise and fall appear to be vertical lines, so it is not possible to determine waveform SR with any accuracy. The TLV9001 waveform does not indicate boost or no boost. The LMV831 waveform is a great waveform to use as an indicator because the input is small, NG is high, and scaling makes rise and fall time measurable. The initial slew rate is consistent with the rest of the rising slew rate, so this section can be used for evaluation. Initial SR of the green oval area is 0.25V/µs. The 10mV VID translates to 14% SR[max] using Figure 3-1. The data sheet value (2V/µs) scaled by 14% is 0.28V/µs. The small signal slew rate of the waveform, 0.25V/µs, closely matches the calculated slew rate, 0.28V/µs. Based on these calculations, the LMV831 device does not have slew boost.

ResultInconclusiveNo Boost
DeviceTLV9001LMV831
NG110
VIN100mV10mV
Initial SRUnknown0.25V/μs

Data sheet SR × Figure 3-1 output

1.8V/μs0.28V/μs
TS321, TL074, TLV9001, OPA4991, OPA2991, OPA991, LMV831, OPA345, LMV821-N, OPA377-Q1, OPA376-Q1, OPA377, OPA376, TLV376, TLV9002 TLV9001 Small Signal WaveformFigure 4-3 TLV9001 Small Signal Waveform
TS321, TL074, TLV9001, OPA4991, OPA2991, OPA991, LMV831, OPA345, LMV821-N, OPA377-Q1, OPA376-Q1, OPA377, OPA376, TLV376, TLV9002 LMV831 Small Signal WaveformFigure 4-4 LMV831 Small Signal Waveform