SLUAA04A june 2020 – may 2023 BQ25150 , BQ25155 , BQ25618 , BQ25619 , TS5A12301E , TS5A3157 , TS5A3159A , TS5A6542
This is a load switch that is used control the case’s output power rail. It also isolates the output capacitance of the buck converter from the signal line while the system is in communication mode. This is an active-low load switch with no Quick Output Discharge (QOD). This device allows for the power path to be the system default so a dead battery case in the case or earbud will not brick the system.