SLUAAM6 November 2022 BQ24190 , BQ24192 , BQ24192I , BQ24195 , BQ24195L , BQ24196 , BQ24292I , BQ24295 , BQ24296 , BQ24297 , BQ24298 , BQ25600 , BQ25600D , BQ25601 , BQ25601D , BQ25606 , BQ25611D , BQ25616 , BQ25618 , BQ25619 , BQ25620 , BQ25622 , BQ25890 , BQ25890H , BQ25892 , BQ25895 , BQ25896 , BQ25898 , BQ25898D
If the application requires USB D+/D- input current limit detection capability, the user needs to check the related specs of a charger IC. Please visit USB D+ D- Input Current Limit Detection for BQ2419x, BQ2429x, BQ2589x, BQ25898x, BQ2560x, and BQ2561x (USB D+ D- Input Current Limit Detection for BQ2419x, BQ2429x, BQ2589x, BQ25898x, BQ2560x, and BQ2561x application note) for the details.
If the application does not require USB D+/D- input current limit, the user can either leave the D+/D- pins open or short the D+/D- pins together. Below are the general guidelines. Please refer to the corresponding data sheet for the specific input current limit settings