SLUAAM6 November 2022 BQ24190 , BQ24192 , BQ24192I , BQ24195 , BQ24195L , BQ24196 , BQ24292I , BQ24295 , BQ24296 , BQ24297 , BQ24298 , BQ25600 , BQ25600D , BQ25601 , BQ25601D , BQ25606 , BQ25611D , BQ25616 , BQ25618 , BQ25619 , BQ25620 , BQ25622 , BQ25890 , BQ25890H , BQ25892 , BQ25895 , BQ25896 , BQ25898 , BQ25898D
As a battery charger designer, one of the most important questions to consider is the control method for the charging system. Shall a microprocessor-controlled charger or a stand-alone charger be used?
The two most popular control methodologies are:
Table 1-1 lists what can be considered when determining the control method for a charger system.
I2C-controlled | Stand-alone | |
---|---|---|
Need real-time control over the charger? | √ | X |
Need the flexibility of charging parameters? | √ | X |
Need to monitor charging parameter values? | √ | X |
Require a host? | Yes | No |
Require software code? | Yes | No |