SLUAAP6 September 2023 UCD3138 , UCD3138064 , UCD3138064A , UCD3138128 , UCD3138128A , UCD3138A , UCD3138A64
It is hard to tell how much size a stack uses statically since the size varies with the code running. There are other things that are stored in RAM as well, for example global variables. If a stack overflow happens, it modifies the others unexpectedly, causing unpredictable problems. Therefore, it is necessary to reserve enough room for STACK. This application note describes two processes to check if a stack overflow happens.
All trademarks are the property of their respective owners.