SLVAE30E February 2021 – March 2021 TPS1H000-Q1 , TPS1H100-Q1 , TPS1H200A-Q1 , TPS1HA08-Q1 , TPS25200-Q1 , TPS27S100 , TPS2H000-Q1 , TPS2H160-Q1 , TPS2HB16-Q1 , TPS2HB35-Q1 , TPS2HB50-Q1 , TPS4H000-Q1 , TPS4H160-Q1
In this application the Smart High Side Switch directly drives the LED and a series resistor that sets the current in the LED string. The Smart High Side Switch provides a constant voltage source, but since the light output is dependent on the current in the LED string pulse width modulation of the switch can be employed to keep the current constant over varying supply voltages. A PWM frequency greater than 120 Hz is applied to the Smart High Side Switch input to vary the duty cycle of switching and modulate the LED current. The choice of Smart High Side Switch is driven primarily by the power dissipation in the switch that occurs while driving the LED current. For directly driving LEDs the primary design factor is the RON of the switch. Ensure that the RON of the switch is low enough that the Smart High Side Switch will not have issues dissipating the power caused by your DC LED current. Single channel or multi-channel devices can be used depending on the total power dissipation in the switch and the heat dissipation of the PCB.