The TPS6594-Q1, TPS6593-Q1, and LP8764-Q1 family of power management integrated circuits (PMICs) include a configurable non-volatile memory (NVM) space. The Scalable PMIC GUI provides the ability to generate a binary image either from an NVM configuration (assembly file) generated from the GUI or generated manually. This document details the hardware setup and steps for uploading the binary image to the NVM of the PMIC.
All trademarks are the property of their respective owners.
The configuration process described in this document writes to the NVM space and is intended to be used in a production line or development setting. This mechanism is not intended to be used in applications since the process impacts the regulator outputs and GPIO functions.
The Scalable PMIC GUI provides a mechanism to generate a binary image which can, in turn, be uploaded to the NVM of the PMIC. The binary is generated from the NVM programming page by selecting Save as Binary Code, as shown in Figure 1-1. See the Scalable PMIC's GUI User’s Guide for instructions on configuring the PMIC and generating an image from that configuration.
Table 1-1 shows examples of entries in the binary file. Each row consists of the page information, the register address, and the data.
Binary Row | Description |
---|---|
0x0004 = 0xa0 | Page 0 entries |
0x00d1 = 0x00 | |
0x0100 = 0x02 | Page 1 entries |
0x014A = 0x06 | |
0x3000 = 0x0A | Page 3 entries |
0x32ff = 0x00 | |
0x405 = 0xff | Page 4 entries |
0x409 = 0xff |
The hardware connections are described in the schematic checklist (see Reference 6). Table 2-1 and Table 2-2 show the required connections associated with NVM configuration.
Pin | Name | Purpose | Connection for Functional Use |
---|---|---|---|
2 | VOUT_LDOVINT | Output pins of internal LDOs for noise decoupling capacitor | Capacitor: Ctyp = 2.2 µF; Vcap > 6.3 V |
3 | VOUT_LDOVRTC | ||
4 | VCCA | Analog input voltage for the internal LDOs and other internal blocks | Capacitor: Cmin = 0.47 µF; Ctyp = 1 µF; Vcap>6.3 V |
5 | REFGND1 | System reference ground | Connect to solid ground plane but not the thermal pad on the top layer. |
6 | REFGND2 | ||
30 | SDA_I2C1, SDI_SPI | I2C or SPI data | Connect to data line of controller. For I2C use resistor value depending upon speed and PCB. |
31 | SCL_I2C1/SCK_SPI | I2C or SPI clock | Connect to clock line of controller. For I2C use resistor value depending upon speed and PCB. |
32 | CS_SPI1 | SPI Chip select | Connect to CS of SPI controller |
33 | SDO_SPI1 | SPI SDO | Connect to SDO of SPI controller |
48 | VIO_IN | Digital supply input for GPIOs and I/O supply voltage | Capacitor: Cmin = 0.47 µF; Ctyp = 1 µF; Vcap > 6.3 V |
57 | Thermal Pad | Power ground, which is also the thermal pad of the package. | Connect to top layer power ground polygon |
Pin | Name | Purpose | Connection for functional use |
---|---|---|---|
20 | VOUT_LDO | Output pin of internal LDO for noise decoupling capacitor | Capacitor: Ctyp = 2.2 µF; Vcap > 6.3 V |
18 | VCCA | Analog input voltage for the internal LDOs and other internal blocks | Capacitor: Cmin = 0.1 µF; Ctyp = 0.47 µF; Vcap > 6.3 V |
19 | AGND1 | System reference ground | Connect to solid ground plane but not the thermal pad on the top layer. |
21 | AGND2 | ||
5 | SDA_I2C1, SDI_SPI | I2C or SPI data | Connect to data line of controller. For I2C use resistor value depending upon speed and PCB. |
4 | SCL_I2C1/SCK_SPI | I2C or SPI clock | Connect to clock line of controller. For I2C use resistor value depending upon speed and PCB. |
2 | CS_SPI(1) | SPI Chip select | Connect to CS of SPI controller |
3 | SDO_SPI(1) | SPI SDO | Connect to SDO of SPI controller |
24 | VIO | Digital supply input for GPIOs and I/O supply voltage | Capacitor: Cmin = 0.1µF; Ctyp = 0.47 µF; Vcap > 6.3 V |
13/29 | PGND | Power Ground | Connect to top layer power ground polygon |
VCCA and VIO must be applied and the serial interface must be accessible to update the NVM. The VIO must not be connected to or dependent upon any GPIO or regulator from the PMIC. Similarly, in the case of an I2C serial interface, the pullup voltage must also be independent of the PMIC. When configuring the NVM via I2C only the I2C1 interface is needed. The I2C2 interface is only used in the application when enabled and utilized solely for the watchdog communication.
The initial PMIC state must also be understood before attempting to configure the NVM. Generally, the PMIC must be in a static or idle state. In some NVM configurations, the PMIC does not power up until the ENABLE pin is activated. Simply holding the ENABLE pin low can be an effective means to hold the PMIC in a known static state.
Also, if the NVM is configured to loop continuously between states polling for a certain condition, this can interfere with the initial steps in the configuration which unlocks the NVM.
Finally, the PMIC does allow for the NVM to be configured while in the safe recovery hardware state. This provides a means to change the NVM in the event that the NVM was erroneously configured and results in an error or shutdown. When defining an NVM, a transition to the safe recovery state is important and must not be omitted. Examples which include the transition to safe recovery are provided in the Scalable PMIC GUI as templates. If a transition is not provided, then the associated interrupts must be serviced for the NVM to be unlocked successfully.
The PMIC has two memory spaces, the register map space and the NVM space. As Figure 3-1 shows, configuring the NVM is done by first writing to the register map through the serial interface and then copying the contents to the NVM. Because the configuration first involves writing to the register map, which controls the regulators and GPIO, there must be no dependency or need to use the PMIC resources. For example, in the PDN-0B implementation(4) the VIO is supplied by a load switch which is controlled by the PMIC GPIO. The dependency upon the GPIO output prohibits NVM configuration since the GPIO controls the VIO, impacting the I2C and corrupting the configuration. In contrast, the TPS6594 EVM(5) provides an independent supply for VIO.