SLVAFT6 September   2024 TPS23521 , TPS23523 , TPS23525

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Existing Design and Challenges
  6. 3Negative Hot-Swap Controller – TPS2352x
  7. 4Output Voltage Clamping with TPS2352x
  8. 5Design Procedure and Implementation
    1. 5.1 Configuring the Current Limit Switch-Over Threshold for TPS2352x
    2. 5.2 Feedback and Control Loop Response
    3. 5.3 Powering the Feedback Amplifier
    4. 5.4 Noise Immunity
  9. 6Test Results
    1. 6.1 Startup
    2. 6.2 NEBS Transient Response
  10. 7Summary
  11. 8References

Configuring the Current Limit Switch-Over Threshold for TPS2352x

TPS2352x has two current limit thresholds as shown in Figure 5-1. This dual-level protection scheme makes sure that the part has a higher chance of riding out voltage steps and other transients due to the higher current limit at low VDS, while protecting the MOSFET during the start into short and hot-short events, by setting a lower current limit threshold for conditions with high VDS. The transition threshold is programmed with a resistor RD that is connected from the drain of the hot-swap FET to the D pin of the TPS23521.

Based on the region of operation, the GATE source capability of TPS23521 varies. In high current limit mode for example, where VDS < VDS,SW, the GATE sourcing current is 400µA vs 20µA at high VDS region. This high GATE current helps to quickly switch ON/OF the external FET to reliably operate in hysteric mode during over-voltage conditions. Considering a peak of 75V input transient from the NEBS standard (Figure 1-2) and the requirement that the voltage to the downstream load does not exceed 62.5V, we have set the VDS,SW to be greater than 12.5V for example, 75V – 62.5V). Accordingly, resistor RD can be selected using Equation 3.

Equation 3. VDS,SW=1.5V×30kΩ+RD30kΩ
 Dual Current Limit in TPS2352xFigure 5-1 Dual Current Limit in TPS2352x