This document covers the usage and capabilities of the Scalable PMIC's graphical user interface (GUI) tool from Texas Instruments. This GUI is intended to be used with the analog EVM Control (AEVM) to evaluate and configure the TPS6594-Q1, TPS6593-Q1, LP8764-Q1, LP8762-Q1, and LP876242-Q1 family of devices.
SimpleLink™ and Launchpad™ are trademarks of Texas Instruments.
Chrome™ is a trademark of Google.
Firefox™ is a trademark of The Mozilla Foundation.
Microsoft Windows,® is a registered trademark of Microsoft Corporation.
Linux® is a registered trademark of Linus Torvalds.
All trademarks are the property of their respective owners.
This tool is based upon GUI Composer and requires the MSP432E401Y SimpleLink™ Ethernet Microcontroller as the analog EVM controller (AEVM), which is integrated in the PMIC EVM and also available with the Launchpad™, see 1 in the Section 11. The AEVM provides a USB interface to the host personal computer (PC) for receiving commands and then communicates with the PMIC using either an I2C or SPI protocol.
The GUI supports multiple devices with a single executable (and single AEVM), which eliminates the need to install multiple GUIs when working with more than one device. Multiple devices are configured in a primary/secondary configuration and the AEVM communicates to each device over the selected shared medium: I2C or SPI.