SLVUBT8B November   2020  – June 2022 LP8764-Q1 , TPS6594-Q1

 

  1.   Scalable PMIC's GUI User’s Guide
  2.   Trademarks
  3. Introduction
  4. Supported Features
  5. Revisions
  6. Overview
  7. Getting Started
    1. 5.1 Finding the GUI
    2. 5.2 Downloading the Required Software
    3. 5.3 Launching the GUI
    4. 5.4 Connecting to a PMIC
  8. Quick-start Page
    1. 6.1 Device Scan Results
    2. 6.2 Configuration and Monitoring
      1. 6.2.1 System Info
      2. 6.2.2 BUCK
      3. 6.2.3 LDO
      4. 6.2.4 GPIO
      5. 6.2.5 Interrupts
      6. 6.2.6 Miscellaneous Settings
      7. 6.2.7 Advanced
  9. Register Map Page
  10. NVM Configuration Page
    1. 8.1 Creating a Custom Configuration
      1. 8.1.1 Static Configuration
      2. 8.1.2 Pre-Configurable Mission States (PFSM)
        1. 8.1.2.1 Creating a State Diagram
        2. 8.1.2.2 Global Settings
        3. 8.1.2.3 Power Sequence
          1. 8.1.2.3.1 Power Sequence Resources and Commands
          2. 8.1.2.3.2 Sub-sequences
          3. 8.1.2.3.3 Power Sequence Editing Tools
        4. 8.1.2.4 Trigger Settings
        5. 8.1.2.5 Trigger Priority List
        6. 8.1.2.6 PFSM Validation
    2. 8.2 Program
      1. 8.2.1 Program an Existing NVM Configuration
      2. 8.2.2 NVM Configuration Special Use Case: Changing the Communication Interface
      3. 8.2.3 Lock Option During NVM Programming
  11. NVM Validation Page
  12. 10Watchdog Page
  13. 11Additional Resources
  14. 12Appendix A: Troubleshooting
    1. 12.1 Hardware Platform Not Recognized
    2. 12.2 PMIC Device Not Found
    3. 12.3 I2C2 is configured but not connected
  15. 13Appendix B: Advanced Topics
    1. 13.1 Scripting Window
  16. 14Appendix C: Known Limitations
  17. 15Appendix D: Migration Topics
    1. 15.1 Migrating from LP8764-Q1 PG1.0 to PG2.0
    2. 15.2 Update the PFSM to Include the PFSM_START State
    3. 15.3 Update Timing Delays
    4. 15.4 Update Trigger Priority and Settings
  18. 16Revision History

NVM Configuration Special Use Case: Changing the Communication Interface

The GUI tool writes the register settings using the identified interface and then uses the bulk programming method to transfer the register settings to the NVM. In the event that the NVM image uses a different interface, then it is important that the device being programmed supports both interfaces. When the GUI writes to the register settings to change the interface (SPI to I2C or I2C to SPI), the GUI will pause and display a prompt, see Figure 8-33, to change the hardware configuration to enable the new interface. This message specifically refers to the EVM, but can be generalized to any hardware configuration where changes are made to transition from I2C to SPI or SPI to I2C.

GUID-20200813-CA0I-JNNC-CGK2-DVFDLWXZCJQ9-low.png Figure 8-33 Interface Change during Programming