SLVUBT8B November 2020 – June 2022 LP8764-Q1 , TPS6594-Q1
The PMIC NVM can be permanently locked, preventing any changes to the NVM configuration. While this is not recommended during development, the feature is supported by the GUI. During the programming, a dialog window appears, see Figure 8-34, with the option to lock the NVM. Once this is done, then the PMIC NVM cannot be changed.
Locking a device is permanent.