SLVUBT8B November 2020 – June 2022 LP8764-Q1 , TPS6594-Q1
Continuing to use the example from Section 15.3, there are additional warnings associated with the triggers. Figure 15-7shows the warnings relative to the trigger to SAFE_RECOVERY.
The trigger priority can be updated in the Trigger Priority List as shown in Figure 15-8. Figure 15-9 shows the immediate trigger feature indicated in the Update Trigger found in the TRIGGER SETTINGS.
Figure 15-10 shows that with these fixes, the PFSM Validation has only one warning, that was discussed in Section 15.3.