SLVUC32B June 2021 – February 2022 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1 , TPS6594-Q1
To achieve a system functional safety level of ASIL-B, the following PDN features are available:
The PDN has an in-line, external power FET, as shown in Figure 3-1, between the input supply and PMICs. The voltage before and after the FET is monitored by the PMIC, and the PMIC controls the FET through the OVPGDRV pin. The FET can quickly isolate the PMICs when an over-voltage event greater than 6 V is detected on the input supply to protect the system from being damaged. This includes all power rails sourced from the FET output. Any power connected upstream from the FET is not protected from over voltage events. In Figure 3-1 the load switches that supply power to the MCU and Main I/O domains, the discrete buck supplying the DDR, and the discrete LDO supplying EFUSE are all connected after the FET to extend the over voltage protection to these processor domains and discrete power resources.
The PMIC internal over voltage and under voltage monitoring and their respective monitoring threshold levels are enabled by default and can be updated through I2C after startup. PMIC power rails connected directly to the processor are monitored by default. Rails supplied through the load switches are not monitored directly. To monitor the load switch output voltage that supplies the MCU I/O of the processor, it is recommended to use the POK monitor built into the VDDSHV0_MCU voltage domain of the processor. The unused feedback pin of BUCK3 on TPS65941212-Q1, FB_B3, is assigned to monitor the VDD_DDR_1V1 voltage supplied by the external BUCK regulator. For monitoring the load switch voltage that supplies the Main I/O, an unused feedback pin of the TPS65941111- Q1 (FB_B3 or FB_B4) can be configured through I2C and connected to the output of the load switch to enable monitoring.
The internal Q&A Watchdog is enabled by default on the primary TPS6594-Q1 device. Once the device is in ACTIVE state, the trigger or Q&A watchdog settings can be configured through the secondary I2C in the device. The primary and secondary I2C CRC is not enabled by default but must be enabled with the I2C_2 trigger described in Table 6-1. Once enabled the secondary I2C is disabled for 2ms. It is recommended to enable I2C CRC and wait a minimum of 2ms before starting the Q&A Watchdog. The steps for configuring and starting the watchdog can be found in the TPS6594-Q1 datasheet. Setting the DISABLE_WDOG signal high on primary TPS6594-Q1 GPIO_8 disables the watchdog timer if this feature needs to be suspended during initial development or is not required in the system.
GPIO_7 of the primary TPS6594-Q1 PMIC is configured as the MCU error signal monitor, and must be enabled though the ESM_MCU_EN register bit. MCU reset is supported through the connection between the primary PMIC nRSTOUT pin and the MCU_PORz of the processor. Lastly, there are two I2C ports between the TPS6594-Q1 and the processor. The first is used for all non-watchdog communication, such as voltage level control, and the second allows the watchdog monitoring to be on an independent communication channel.
There is an option to use the primary TPS6594-Q1 EN_DRV pin to indicate an error has been detected and the system is entering SAFE state. This signal can be utilized if the system has some additional external circuitry that needs to be driven by an error event. In this PDN, the EN_DRV is not utilized, but still available.