SLVUC32B June   2021  – February 2022 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1 , TPS6594-Q1

 

  1.   Trademarks
  2. 1Introduction
  3. 2Device Versions
  4. 3Processor Connections
    1. 3.1 Power Mapping
    2. 3.2 Control Mapping
  5. 4Supporting Functional Safety Systems
    1. 4.1 Achieving ASIL-B System Requirements
    2. 4.2 Achieving up to ASIL-D System Requirements
  6. 5Static NVM Settings
    1. 5.1  Application-Based Configuration Settings
    2. 5.2  Device Identification Settings
    3. 5.3  BUCK Settings
    4. 5.4  LDO Settings
    5. 5.5  VCCA Settings
    6. 5.6  GPIO Settings
    7. 5.7  Finite State Machine (FSM) Settings
    8. 5.8  Interrupt Settings
    9. 5.9  POWERGOOD Settings
    10. 5.10 Miscellaneous Settings
    11. 5.11 Interface Settings
    12. 5.12 Multi-Device Settings
    13. 5.13 Watchdog Settings
  7. 6Pre-Configurable Finite State Machine (PFSM) Settings
    1. 6.1 Configured States
    2. 6.2 PFSM Triggers
    3. 6.3 Power Sequences
      1. 6.3.1 TO_SAFE_SEVERE and TO_SAFE
      2. 6.3.2 TO_SAFE_ORDERLY and TO_STANDBY
      3. 6.3.3 ACTIVE_TO_WARM
      4. 6.3.4 ESM_SOC_ERROR
      5. 6.3.5 PWR_SOC_ERROR
      6. 6.3.6 MCU_TO_WARM
      7. 6.3.7 TO_MCU
      8. 6.3.8 TO_ACTIVE
      9. 6.3.9 To Suspend-to-RAM (TO_S2R)
  8. 7Impact of NVM Changes
  9. 8References
  10. 9Revision History

Control Mapping

Figure 3-2 shows the digital control signal mapping between processor and PMIC devices. For the two PMIC devices to work together, the primary PMIC and secondary PMIC must establish an SPMI communication channel. This allows the two TPS6594-Q1 to synchronize their internal Pre-Configurable State Machines (PFSM) so that they operate as one PFSM across all power and digital resources. The GPIO_5 and GPIO_6 pins on the TPS6594-Q1 are assigned for this functionality. In addition, the primary PMIC LDOVINT pin is connected to the secondary PMIC ENABLE input to correctly initiate the PFSM.

Other digital connections from the TPS6594-Q1 devices to the processor provide error monitoring, processor reset, processor wake up, and system low-power modes. Specific GPIO pins have been assigned to key signals in order to ensure proper operation during low power modes when only a few GPIO pins remain operational.

The digital connections shown in Figure 3-2 allow system features including MCU-only MCU Safety Island and suspend-to-RAM low power modes, functional safety up to ASIL-D, compliant dual voltage SD card operation, and LPDDR4x integration.

GUID-20210215-CA0I-8J03-7JNF-BHNV1JTFXRBT-low.gif Figure 3-2 TPS6594-Q1 Digital Connections
Note: The PMIC voltage domain of an IO can be different depending upon configuration. When configured as an input GPIO3 and GPIO4 are in the VRTC domain. When configured as an output, GPIO3 and GPIO4 are in the VINT domain.
Note: In addition to the I2C signals, four additional signals are open-drain outputs and require a pullup to a specific power rail. Please refer to Table 3-2 for a list of the signals and the specific power rail.
Table 3-2 Open-drain signals and Power Rail
PDN Signal Pullup Power Rail
H_MCU_INTn VDD_MCUIO_3V3
H_MCU_PORz_1V8 VDA_MCU_1V8
H_SOC_PORz_1V8 VDA_MCU_1V8
H_DDR_RET_1V1 VDD_DDR_1V1_REG
H_WKUP_I2C0 VDD_MCUIO_3V3
H_MCU_I2C0_SCL/SDA VDD_MCUIO_3V3

Please use Table 3-3 as a guide to understand GPIO assignments required for each PDN system feature. If the feature listed is not required, the digital connection can be removed; however, the GPIO pin is still configured per NVM defined default function shown. After the processor has booted up, system software can potentially reconfigure an unused GPIO to support a new function. This is possible as long as that function is only needed after boot and default function does not cause any conflicts with normal operations (for example, two outputs driving same net). For details on how functional safety related connections help achieve functional safety system-level goals, see Section 4.

Table 3-3 Digital Connections by System Feature
Device GPIO Mapping System Features
PMIC Pin NVM Function PDN Signals Active SoC Functional Safety MCU - only and MCU-Safety Island Suspend-to-RAM SD Card
TPS65941212-Q1 nPWRON/ ENABLE Enable SOC_PWR_ON Required
INT INT H_MCU_INTn Required
nRSTOUT nRSTOUT H_MCU_PORz_1V8 Required Required
SCL_I2C1 SCL_I2C1 H_WKUP_I2C0 Required
SDA_I2C1 SDA_I2C1 H_WKUP_I2C0 Required
GPIO_1 SCL_I2C2 H_MCU_I2C0_SCL Required
GPIO_2 SDA_I2C2 H_MCU_I2C0_SDA Required
GPIO_3 GPO EN_MCU3V3IO_LDSW Required
GPIO_4 LP_WKUP1 H_WAKE_PMIC Required
GPIO_5 SCLK_SPMI LEOA_SCLK Required
GPIO_6 SDATA_SPMI LEOA_SDATA Required
GPIO_7 nERR_MCU PMICA_SAFETY_ERRn Required
GPIO_8 DISABLE_WDOG PMICA_GPIO8 (2) (2)
GPIO_9 GPI PMICA_GPIO9(3)
GPIO_10 WKUP1 PMIC_POWER_EN1 Required
GPIO_11 nRSTOUT_SOC H_SOC_PORz_1V8 Required
TPS65941111-Q1 nPWRON/ENABLE ENABLE VINT_LEOA_1V8 Required
nINT nINT H_MCU_INTn
nRSTOUT nRSTOUT Unused
SCL_I2C1 SCL_I2C1 H_WKUP_I2C0 Required
SDA_I2C1 SCL_I2C1 H_WKUP_I2C0 Required
GPIO_1 GPI Unused(3)
GPIO_2 GPI SEL_SDIO_3V3_1V8n(1) Required
GPIO_3 GPO EN_DDR_BUCK
GPIO_4 GPO H_DDR_RET_1V1 Required
GPIO_5 SCLK_SPMI LEOA_SCLK Required
GPIO_6 SDATA_SPMI LEOA_SDATA Required
GPIO_7 GPI Unused(3)
GPIO_8 GPI Unused(3)
GPIO_9 GPO EN_EFUSE_LDO(3)
GPIO_10 WKUP2 Unused(3)
GPIO_11 GPO EN_3V3IO_LDSW Required
This pin is an input with an internal pulldown enabled. A rising edge on this GPI initiates the FSM trigger and associated sequence. The sequence configures LDO1 to bypass mode, supplying 3.3 V. A falling edge triggers an alternate sequence which configures LDO1 to LDO mode, supplying 1.8 V. See also Table 6-1
If it is desired to disable the watchdog through hardware, GPIO_8 is required and must be set high by the time nRSTOUT goes high. After nRSTOUT is high, the watchdog state is latched and the pin can be configured for other functions through software.
This GPIO is not required for power sequencing or PMIC functionality and can be configured by software for a different purpose if desired.