To setup the software configuration,
follow the instructions below.
- Open the Application Customization Tool and select
Configuration Index 1 or 3 for Question 1 (A figure with a BQ block
included).
- Fill out the questionnaire
from Q2 to Q10. For more details on each question configuration, refer to
Section 3.4.3. All the questions must be filled out to flash or export.
- Questions 11 through 18
pertain to Battery Charger (BQ) settings.
- For Question 11, select
BQ25756.
- For Question 12, select the
INDPM configuration for the BQ25756.
- For example, if the
user selects 5% - INDPM is set to 5% above the negotiated PD
Contract Current and TPS26750 negotiates a PD contract at
3A, then the INDPM is set to 3.15A.
- This questionnaire
configures register 0x06 - IAC_DPM of the BQ25756.
- For Question 13, select the
VINDPM configuration for the BQ25756.
- For example, if the
user selects 5% - VINDPM is set to 5% below the negotiated PD
Contract Voltage and TPS26750 negotiates a PD contract at
5V, the VINDPM is set to 4.75V.
- This questionnaire
configures register 0x08 - VAC_DPM of the BQ25756.
- For question 14, enter the FB
Voltage Regulation Limit in units of Voltage (1.504V through 1.566V,
2mV/bit).
- This questionnaire
configures register 0x00 - VFB_REG of the BQ25756.
- For question 15, enter the
Charge Current Limit in units of Ampere (0.4A through 20A, 50mA/bit)
- This questionnaire
configures register 0x02 - ICHG_REG of the BQ25756.
- For question 16, enter the
Charge Termination Current Limit in units of Ampere (0.25A through 10A,
50mA/bit).
- This questionnaire
configures register 0x12 - ITERM of the BQ25756.
- For question 17, enter the
Precharge Current Limit in units of Ampere (0.25A through 10A, 50mA/bit).
- This questionnaire
configures register 0x10 - IPRECHG of the BQ25756.
- For question 18, enter the
Dead Battery Clear Threshold in units of Voltage (2.88V through 19.2V,
64mV/bit).
- This questionnaire
configures register 0x27 - Global System Configuration of the
TPS26750 and sets the Enable Dead Battery Clear [111] field
to '1'.
- Upon boot-up from
dead battery mode (The TPS26750 receives power from VBUS first
instead of VIN_3V3), the TPS26750 reads register 0x33 - VBAT_ADC of
the BQ25756.
- If VBAT voltage is
greater or higher than set threshold in Q18, then the TPS26750
automatically clears the dead battery flag, otherwise the dead
battery flag remains. Refer to the TPS26750 Technical Reference
Manual for details.
- For flashing the
configuration to the TPS26750EVM or exporting the binary, refer to Section 3.4.6.