Now, that the EVM hardware setup and GUI
installation is complete, the EVM can now be connected to the GUI. The following
steps outline how to connect the EVM to GUI:
- With the EVM connected to the PC, open the GUI.
The home page or landing page of the GUI is shown in Figure 4-2.
- Program EVM with latest software
by clicking on File -> Program Device (See )Figure 4-3. This needs to be done the first time the user sets up the EVM, as a software
update can have been released since the EVM was initially programmed.
- Select the appropriate GUI variant from the six
options for the EVM (see Figure 4-4).
- The GUI attempts to connect with
EVM. The GUI displays the following once successfully connected. If there is no
successful connection, then double check the correct steps are followed in Section 2.3.
- Once successfully connected, click on Quick
Start to open the Channel Config. page under Features section to open
the main control page.
- The GUI setup is now complete. The following
section provides an overview of the GUI and how to use the GUI to control
EVM.