SLYT820 February   2022 AMC22C11 , AMC22C12 , AMC23C10 , AMC23C11 , AMC23C12 , AMC23C12-Q1 , AMC23C14

 

  1. 1Introduction
  2. 2Introduction to electric motor drives
  3. 3Understanding fault events in electric motor drives
  4. 4Achieving reliable detection and protection in electric motor drives
  5. 5Use case No. 1: Bidirectional in-phase overcurrent detection
  6. 6Use case No. 2: DC+ overcurrent detection
  7. 7Use case No. 3: DC– overcurrent or short-circuit detection
  8. 8Use case No. 4: DC-link (DC+ to DC–) overvoltage and undervoltage detection
  9. 9Use case No. 5: IGBT module overtemperature detection

Use case No. 1: Bidirectional in-phase overcurrent detection

Figure 5-1 shows how AMC23C12 can be used for bidirectional in-phase overcurrent detection.

GUID-20211215-SS0I-KHGJ-PTDM-T2FDPQBV8ZRH-low.png Figure 5-1 Bidirectional in-phase overcurrent detection.

In a fully operational three-phase AC motor-drive system, the sum of three-phase current to the AC motor should be zero, regardless of braking or running conditions (that is, IA + IB + IC = 0).

Calculating the third-phase current in low- to mid-end motor drives from measured current on two phases can help reduce costs. I recommend monitoring the current on the third phase to detect any electrical fault events. While you could place a current sensor on the third phase with an isolated amplifier or isolated modulator, you could also use a reinforced isolated window comparator AMC23C12 for simplicity, cost-effectiveness and solution size. The AMC23C12offers bidirectional overcurrent detection with an integrated window comparator.

As shown in location 1 of Figure 5-1, a shunt resistor produces a voltage drop that the AMC23C12 reinforced window comparator senses. The AMC23C12 has an open-drain output, OUT, which actively pulls low when the input voltage exceeds the pre-defined threshold values of the voltage on the reference pin for the purposes of overcurrent detection. Figure 5-2 shows an overcurrent event output waveform.

For both overcurrent and short-circuit detection, you can use the AMC23C14 dual window comparator.

Figure 5-2 AMC23C12 output waveform.