SLYT820 February   2022 AMC22C11 , AMC22C12 , AMC23C10 , AMC23C11 , AMC23C12 , AMC23C12-Q1 , AMC23C14

 

  1. 1Introduction
  2. 2Introduction to electric motor drives
  3. 3Understanding fault events in electric motor drives
  4. 4Achieving reliable detection and protection in electric motor drives
  5. 5Use case No. 1: Bidirectional in-phase overcurrent detection
  6. 6Use case No. 2: DC+ overcurrent detection
  7. 7Use case No. 3: DC– overcurrent or short-circuit detection
  8. 8Use case No. 4: DC-link (DC+ to DC–) overvoltage and undervoltage detection
  9. 9Use case No. 5: IGBT module overtemperature detection

Use case No. 5: IGBT module overtemperature detection

As shown in Figure 9-1, a negative temperature coefficient thermistor (NTC) is typically placed inside the IGBT module for the detection of long-term overload conditions. These NTC terminals are routed to the main power board, where the AMC23C14 can be used for overtemperature detection.

GUID-20211215-SS0I-WVV5-TH8B-7RFN3CLTFTCL-low.png Figure 9-1 IGBT module overtemperature detection.

Figure 9-2 shows the output waveform for an overtemperature event, where OUT2 pulls high when the input voltage exceeds the threshold values defined by the internal 300-mV reference. The reference pin of the AMC23C14 connects to a 100-μA current source that can bias the NTC.

GUID-20211215-SS0I-HBGK-LQHL-2LPNH0GKNZPZ-low.png Figure 9-2 AMC23C14 output waveform.

As the demand to improve system reliability and the adoption of faster switching devices proliferates, the AMC23C14 family of low-latency reinforced isolated comparators solves the critical need for accurate and fast detection in electric motor drives