SLYY193C january 2023 – april 2023 LMQ61460-Q1 , TPS54319 , TPS62088 , TPS82671 , UCC12040 , UCC12050
In a buck converter, reverse recovery occurs when the high-side MOSFET turns on while the body diode of the low-side MOSFET is conducting current, thus forcing the low-side diode current to rapidly transition to the high-side MOSFET. In the process of this transition, a current is required to remove the low-side diode minority charge causing a direct switching loss, see Equation 4.
One of the best approaches to reduce the impact of diode reverse recovery is to reduce the stored charge (QRR) through optimized MOSFET design, or to reduce or eliminate the rising edge dead time, thus negating the impact of the loss completely.