This white paper explores the 85°C/85% RH accelerated life test, its impact on RH sensors, and ultimately how to address conflicts when the same design needs both 85°C/85% tests and RH sensors.
Consumers expect their electronic systems to last for a specific period of time, either because they have historically, or because the manufacturer provided a specific lifetime warranty. Enabling a system to operate beyond these expectations gives consumers confidence in the product and its manufacturer, and can engender brand loyalty. In products such as heating, ventilation and air-conditioning systems or vehicles, consumers expect product lifetimes to extend beyond 10 years, a phenomenon that is ultimately putting pressure on system developers to ensure reliable designs – normally through extended testing.
The need for improved reliability of systems has also driven adoption of relative humidity (RH) sensors that provide information about the moisture content in the air. Moisture in the environment can create short circuits between electrical components, influence other components such as CO2 or pressure sensors, or can simply change the efficiency of systems designed to control air quality and temperature. The most common types of humidity sensors leverage a polymer to interact chemically with moisture in the air, and then quantify the moisture absorption based on a resistance or capacitance value. While these types of RH sensors are ultimately effective at the task of evaluating moisture content in a system, this chemical interaction with the environment leads to unique challenges compared to other components, especially when it comes to accelerated life testing.
Accelerated life tests, or tests that stress devices to accelerate fail mechanisms, help evaluate design behaviors during the electronic system development process, as illustrated in Figure 1. Accelerated life testing is important in products or systems that have long life cycles, because studying the behavior for the duration of that lifetime is not usually practical or feasible.
Two such tests – defined by Joint Electron Device Engineering Council (JEDEC) JESD22-A110 and JESD22-A101 standards, respectively – are the biased highly accelerated temperature and humidity stress test (BHAST) and the steady-state temperature humidity bias (THB) life test. These tests are known as 85°C/85% RH tests or 85/85 tests, meaning that the testing exceeds 85°C and 85% RH at the same time.
A BHAST requires 96 hours of electrical biasing while maintaining 130°C and 85% RH, in addition to a vapor pressure of 33.5 PSIA with the goal of accelerating corrosion within the device. In semiconductors, the BHAST test helps ensure that devices will continue operating electrically over extended product life cycles, despite exposure to humid environments, by accelerating the penetration of moisture into the package and die surface.
A THB life test is very similar, with the exclusion of pressure. The stress usually activates the same failure mechanism as a BHAST but with a lower acceleration factor; thus, units are subjected to a longer stress time of 1,000 hours at 85°C and 85% RH.
BHAST and THB tests can be equally useful in system testing. In a chip these accelerated life tests can simulate moisture ingress into a plastic package. In a full system the printed circuit board, connections and other materials can also be affected by humidity in the air over time.[KA1]