Generally, TI differential clock
buffer families have two different DC biasing options, internal bias with small DC
offset or internal DC bias with hysteresis. Both DC bias options are used to set
the outputs to low state and avoid glitches on the outputs when there is loss of
signal or clock. Figure 4-1 and Figure 4-2 shows both biasing techniques.
Figure 4-1 Internal DC Bias Offset
Architecture Figure 4-2 Internal DC Bias with
Hysteresis
Things to consider before opting for
internal and external DC bias.
- Check if the part has internal DC
bias option, otherwise use external bias through a voltage divider. Internal
bias at the inputs can be checked by probing the inputs with a high impedance on
scope. Some TI devices offer VAC _REF pin for external biasing which can be used
instead of voltage divider.
- In case of internal DC bias with
an offset at the input. External DC bias is recommended when using sine wave
input to avoid duty cycle distortion on the output. Duty cycle distortion is
result of sine wave imbalance at the switching threshold as shown in Figure 4-3.
- When using large input signals at
the differential input stage. Make sure that internal bias is good enough that
the low or high level of the input signal doesn’t violate the input absolute
maximum values in the data sheet. Otherwise re-bias the input signal with an
external bias to avoid VIH and VIL absolute maximum values violations.
- Refer to device data sheet for
specific input termination needs due to any specific input requirements.