SNOAA18A January   2019  – September 2024 TLV3011 , TLV3011-Q1 , TLV3011B , TLV3011B-Q1 , TLV3012-Q1 , TLV3012B , TLV3012B-Q1 , TLV4021 , TLV4041

 

  1.   1
  2.   2
  3.   Trademarks

Design Goals

Battery Voltage Levels (VBAT) Comparator Output Status (OUT)
Undervoltage (VLOW) Start-Up Operating Voltage (VHIGH) Low Battery Normal Operation
< 2.000V > 2.034V VOL < 0.4V VOH = VPU = 1.8V

Design Description

This undervoltage, protection circuit uses one comparator with a precision, integrated reference to create an alert signal at the comparator output (OUT) if the battery voltage sags below 2.0V. The undervoltage alert in this implementation is ACTIVE LOW. So when the battery voltage drops below 2.0V, the comparator output goes low, providing as an alert signal to whatever device is monitoring the output. Hysteresis is integrated in the comparator such that the comparator output will return to a logic high state when the battery voltage rises above 2.034V. This circuit utilizes an open-drain output comparator in order to level shift the output high logic level for controlling a digital logic input pin. For applications needing to drive the gate of a MOSFET switch, a comparator with a push-pull output is preferred.

Design Notes

  1. Select a comparator with a precision, integrated reference.
  2. Select a comparator with an open-drain output stage for level-shifting.
  3. Select values for the resistor divider so the critical undervoltage level occurs when the input to the comparator (IN) reaches the comparator's negative-going input threshold voltage (VIT-).

Design Steps

  1. Calculate the resistor divider ratio needed so the input to the comparator crosses VIT- when VBAT sags to the target undervoltage level (VLOW) of 2.0V. VIT- from the TLV4021R1 data sheet is 1.18V.
    V IT - = R 2 ( R 1 + R 2 ) × V LOW
    R 2 ( R 1 + R 2 ) = V IT - V LOW = 1 . 18   V 2 . 00   V = 0 . 59
  2. Confirm that the value of VLOW, the voltage level where the undervoltage alert signal is asserted, is 2.0V.
    V LOW = R 1 + R 2 R 2 × V IT - = 1 0 . 59 × 1 . 18   V = 2 . 0   V
  3. Select values for R1 and R2 that yield the resistor divider ratio of 0.59 by using the following equation or using the online tool Voltage Divider Calculator.
    If using the following equation, choose a value for R2 in the Mega-ohm range and calculate for R1. In this example, a value of 1.54 M was chosen for R2.
    R 1 = R 2 V LOW V IT - - 1 =   1 . 54   2   V 1 . 18   V - 1 = 1 . 07  
  4. Verify that the current through the resistor divider is at least 100 times higher than the input bias current of the comparator. The resistors can have high values to minimize power consumption in the circuit without adding significant error to the resistor divider.
  5. Calculate VHIGH, the battery voltage where the undervoltage alert signal is de-asserted (returns to a logic high value). When the battery voltage reduces below the 2.0V level or is ramping up at initial start-up, the comparator input needs to exceed (VIT+), the positive-going input threshold voltage for the output to return to a logic high. VIT+ from the TLV4021R1 data sheet is 1.20V.
    V HIGH =   R 1 + R 2 R 2 × V IT + = 1 . 07   + 1 . 54   1 . 54   × 1 . 20 V = 2 . 034   V

Design Simulations

DC Simulation Results

Transient Simulation Results

References

Texas Instruments, High-Side Current Sensing with Comparator Circuit, analog engineer's circuit

Design Featured Comparator

TLV4021R1
VS 1.6V to 5.5V
VinCM Rail-to-rail
VOUT Open Drain
Integrated Reference 1.2V ±1% over temperature
Hysteresis 20mV
IQ 2.5µA
tPD(HL) 450ns
TLV4021R1

Design Alternate Comparator

TLV4041R1 TLV3011
VS 1.6V to 5.5V 1.8V to 5.5V
VinCM Rail-to-rail Rail-to-rail
VOUT Push-Pull Open Drain
Integrated Reference 1.2V ±1% over temperature 1.242 ±1% room temperature
Hysteresis 20mV NA
IQ 2.5µA 2.8µA
tPD(HL) 450ns 6µs
TLV4041R1 TLV3011