The inductor are selected according to three
parameters: calculated inductance value (LM), RMS inductor current and the
maximum peak inductor current.
- The inductance is selected to be the standard 1.5µH, which is a common value
that is commercially available.
- The saturation current of the inductor should be larger than the
maximum current limit of the converter device selected. If the inductor becomes saturated,
the components can be damaged and the converter cannot operate correctly .
- With the ripple ignored, the inductor RMS current can be approximated by the
average inductor current, which is estimated to be 3.6 A. The inductor RMS current rating
should be higher than the estimated RMS current and keep the inductor temperature within a
reasonable level based on the application.
For this design example, the inductor is selected
to have an inductance value of 1.5µH, a saturation current limit of 15 A, and a 20°C
temperature rise at 10A RMS.