SNVA994A February 2022 – March 2023 LM5157 , LM5157-Q1 , LM51571-Q1 , LM5158 , LM5158-Q1 , LM51581 , LM51581-Q1
Three main parameters are considered when selecting the inductance value of primary winding: primary winding current ripple ratio (ILRR), falling slope of the transformer current and the RHPZ frequency (ωZ_RHP). Finding a balance between these three parameters helps to simplify the rest of the design process.
A maximum ripple ratio between 30% and 70% results in a good balance of the total power loss of the transformer, matching the down slope of the transformer current to the internal slope compensation and the increasing the right half plane zero frequency. The maximum ripple ratio of the inductor current is set to 60%. In CCM operation, the maximum primary winding ripple current occurs when the supply voltage is at the maximum value. For this application we choose CCM at the minimum input voltage and DCM for the higher voltage range. The primary winding inductance value for CCM operation is calculated using Equation 6.
where
The primary winding inductance is selected to be 8µH. The primary winding ripple current and primary winding peak current are calculated using Equation 7 and Equation 8, respectively. The peak primary winding current occurs at the minimum supply voltage.
ILPEAK is used to properly size the current sense resistor. Table 3-1 summarizes the key parameters of selected transformer.
Parameter | Value |
---|---|
Turns Ratio (NP:NS1:NS2:NS3:NS4) | 1:1.2:2.4:2.4:2.4 (5:6:12:12:12) |
Primary winding inductance (LM) | 8 µH |
Primary winding saturation current (ISAT) | 5.5 A |