SPRAD12A July   2022  – February 2023 F29H850TU , F29H859TU-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SJ-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   Abstract
  2.   Trademarks
  3. Introduction
  4. SysConfig
  5. Time-Base (TB) Submodule
    1. 3.1 Setting the Frequency
    2. 3.2 Applying a Phase Shift
    3. 3.3 Setting up the Synchronization (Sync) Scheme
  6. Counter-Compare (CC) and Action-Qualifier (AQ) Submodules
    1. 4.1 Calculating the Duty Cycle
  7. Deadband (DB) Submodule
    1. 5.1 Setting up Signal Pairs
  8. Verifying the Output
    1. 6.1 Checking the Duty Cycle and Dead-Time Insertion
    2. 6.2 Checking the Phase Shift Applied
  9. Trip-Zone (TZ) and Digital Compare (DC) Submodules
    1. 7.1 Drive Outputs Low for an ePWM Cycle Upon Trip Condition Set Through CMPSS
    2. 7.2 Drive Outputs Low Until Cleared Through Software Upon Trip Condition set Through GPIO
  10. Event-Trigger (ET) Submodule
    1. 8.1 Setting Up Time-Base Interrupts
  11. Global Load
    1. 9.1 Applying Global Loading and One-Shot Load Feature
    2. 9.2 Linking the ePWM Modules
    3. 9.3 Updating Action Qualifier Settings and Counter Compare Values Through Global Loading
  12. 10Summary
  13. 11References
  14. 12Revision History

SysConfig

As mentioned in the abstract, this application report utilizes SysConfig in order to configure the ePWM module along with the other required components. Within SysConfig, each submodule of the ePWM module has its own grouping, including a Global Load and HRPWM grouping. If more general information about SysConfig is required, see the items listed in GUID-647B8A38-4C5C-4DC7-84EB-98340DDE5560.html#GUID-647B8A38-4C5C-4DC7-84EB-98340DDE5560.

Aside from being able to configure each of the submodules, the ePWM modules also have a "Global Parameters" section at the very top. These settings are used to enable information/warnings as well as affect how the code is being generated from the ePWM module.
Figure 2-1 SysConfig- ePWM Module: Global Parameters
Note: By default, SysConfig only generates a predefined set of code along with code from any settings that are not in the default state for the ePWM module. However, these settings can be changed within the Global Parameters section.