SPRADI6 May 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Traditionally, the detection of the PC pointer is achieved by jumping to a specified function address through the self-test program and then comparing the returned address with the preset address. If the addresses are the same, the self-check passes. The essence of this check is to verify the correctness of function jumps.
In actual applications, watchdogs are enabled and watchdog feeding operations are performed in fixed-frequency interrupts. Therefore, entering the watchdog interrupt to perform feeding indicates that the PC pointer is functioning properly. If the PC pointer fails, a reset caused by watchdog timer overflow occurs, achieving the same protective purpose. Therefore, the PC pointer is usually not individually self-checked. The detection of the PC pointer can be combined with enabling the watchdog and explained in the documentation provided to the certification agency.