SPRS698J November 2010 – September 2021 TMS320F28062 , TMS320F28062-Q1 , TMS320F28062F , TMS320F28062F-Q1 , TMS320F28063 , TMS320F28064 , TMS320F28065 , TMS320F28066 , TMS320F28066-Q1 , TMS320F28067 , TMS320F28067-Q1 , TMS320F28068F , TMS320F28068M , TMS320F28069 , TMS320F28069-Q1 , TMS320F28069F , TMS320F28069F-Q1 , TMS320F28069M , TMS320F28069M-Q1
PRODUCTION DATA
The McBSP module has the following features:
where CLKSRG source could be LSPCLK, CLKX, or CLKR. Serial port performance is limited by I/O buffer switching speed. Internal prescalers must be adjusted such that the peripheral speed is less than the I/O buffer speed limit.
See Section 8.9 for maximum I/O pin toggling speed.
On the 80-pin package, only the clock-stop mode (SPI) of the McBSP is supported.
Figure 8-38 shows the block diagram of the McBSP module.
Table 8-29 provides a summary of the McBSP registers.
NAME | McBSP-A ADDRESS | TYPE | RESET VALUE | DESCRIPTION |
---|---|---|---|---|
Data Registers, Receive, Transmit | ||||
DRR2 | 0x5000 | R | 0x0000 | McBSP Data Receive Register 2 |
DRR1 | 0x5001 | R | 0x0000 | McBSP Data Receive Register 1 |
DXR2 | 0x5002 | W | 0x0000 | McBSP Data Transmit Register 2 |
DXR1 | 0x5003 | W | 0x0000 | McBSP Data Transmit Register 1 |
McBSP Control Registers | ||||
SPCR2 | 0x5004 | R/W | 0x0000 | McBSP Serial Port Control Register 2 |
SPCR1 | 0x5005 | R/W | 0x0000 | McBSP Serial Port Control Register 1 |
RCR2 | 0x5006 | R/W | 0x0000 | McBSP Receive Control Register 2 |
RCR1 | 0x5007 | R/W | 0x0000 | McBSP Receive Control Register 1 |
XCR2 | 0x5008 | R/W | 0x0000 | McBSP Transmit Control Register 2 |
XCR1 | 0x5009 | R/W | 0x0000 | McBSP Transmit Control Register 1 |
SRGR2 | 0x500A | R/W | 0x0000 | McBSP Sample Rate Generator Register 2 |
SRGR1 | 0x500B | R/W | 0x0000 | McBSP Sample Rate Generator Register 1 |
Multichannel Control Registers | ||||
MCR2 | 0x500C | R/W | 0x0000 | McBSP Multichannel Register 2 |
MCR1 | 0x500D | R/W | 0x0000 | McBSP Multichannel Register 1 |
RCERA | 0x500E | R/W | 0x0000 | McBSP Receive Channel Enable Register Partition A |
RCERB | 0x500F | R/W | 0x0000 | McBSP Receive Channel Enable Register Partition B |
XCERA | 0x5010 | R/W | 0x0000 | McBSP Transmit Channel Enable Register Partition A |
XCERB | 0x5011 | R/W | 0x0000 | McBSP Transmit Channel Enable Register Partition B |
PCR | 0x5012 | R/W | 0x0000 | McBSP Pin Control Register |
RCERC | 0x5013 | R/W | 0x0000 | McBSP Receive Channel Enable Register Partition C |
RCERD | 0x5014 | R/W | 0x0000 | McBSP Receive Channel Enable Register Partition D |
XCERC | 0x5015 | R/W | 0x0000 | McBSP Transmit Channel Enable Register Partition C |
XCERD | 0x5016 | R/W | 0x0000 | McBSP Transmit Channel Enable Register Partition D |
RCERE | 0x5017 | R/W | 0x0000 | McBSP Receive Channel Enable Register Partition E |
RCERF | 0x5018 | R/W | 0x0000 | McBSP Receive Channel Enable Register Partition F |
XCERE | 0x5019 | R/W | 0x0000 | McBSP Transmit Channel Enable Register Partition E |
XCERF | 0x501A | R/W | 0x0000 | McBSP Transmit Channel Enable Register Partition F |
RCERG | 0x501B | R/W | 0x0000 | McBSP Receive Channel Enable Register Partition G |
RCERH | 0x501C | R/W | 0x0000 | McBSP Receive Channel Enable Register Partition H |
XCERG | 0x501D | R/W | 0x0000 | McBSP Transmit Channel Enable Register Partition G |
XCERH | 0x501E | R/W | 0x0000 | McBSP Transmit Channel Enable Register Partition H |
MFFINT | 0x5023 | R/W | 0x0000 | McBSP Interrupt Enable Register |