SSZT054 october 2022 TPS7H5001-SP , TPS7H5002-SP , TPS7H5003-SP , TPS7H5004-SP , TPS7H5005-SEP , TPS7H5006-SEP , TPS7H5007-SEP , TPS7H5008-SEP
Satellite power design has a complex set of trade-offs given that the design has more variables, and the number of semiconductor options are significantly smaller than those in commercial applications. A satellite’s primary power supply is especially important, since if it fails, there’s little to no opportunity for repair. And with the advancement of space-grade high-performance field-programmable gate arrays, satellites now have significantly higher local computing power, increasing overall power demands.
When developing any satellite electrical power system (EPS), two of the most important trade-offs are the overall thermal design and the mission profile radiation requirements.
Component selection, topology selection and switching frequency are all vital when determining the efficiency of a switched-mode power supply (SMPS). The thermal load of the system directly correlates to the efficiency of the power supplies and the dissipation of power losses throughout the satellite.
A satellite’s EPS must step down the voltages from the energy generation solar array portion of the system (typically 100 V ±50%) to the battery storage portion (typically 28 V ±20%), and then again to the clean point-of-load power supply (<5 V) for satellite payload cards such as single board computers, instrumentation or communication cards, or radar or communication cards. At each of these conversion stages, achieving the highest possible efficiency will help reduce power losses, as space power losses have far wider overall system and weight implications.
One technique to improve efficiency is synchronous rectification, where replacing a conventional power diode with a gate-controlled transistor significantly reduces the conduction loss of the power path. The forward characteristic of diodes, particularly those suitable for handling the current targeted by newer SMPS designs, often results in a larger voltage drop during the on-state. On the other hand, the synchronous rectification transistor is typically a field-effect transistor with a low on-state resistance, leading to much lower conduction losses at the same current level.
In a satellite’s EPS design, pulse-width modulation (PWM) controller-based architectures provide the greatest flexibility to support a range of power-supply topologies at the highest efficiency levels. The radiation-hardened TPS7H5001-SP PWM controller family and radiation-tolerant TPS7H5005-SEP PWM controller family both support synchronous rectification, configurable dead time and other integrated features that enable designers to create smaller and more efficient isolated or non-isolated power supplies. An adjustable duty-cycle limit of 50%, 75% or 100% allows designers to use a single controller in the implementation of DC/DC converter topologies and integrated synchronous rectification outputs enable fully synchronous versions of each topology without additional external circuitry, offering overall system size benefits. Configurable dead time helps optimize power converter efficiency, particularly for gallium nitride (GaN) power semiconductor-based designs. An adjustable leading-edge blank time enables configuration of the controller’s internal current sense based on the specific converter parasitic inductances and capacitances, as well as those for the printed circuit board or power module substrates.
Table 1 compares the different devices.
Feature | TPS7H5001-SP TPS7H5005-SEP |
TPS7H5002-SP TPS7H5006-SEP |
TPS7H5003-SP TPS7H5007-SEP |
TPS7H5004-SP TPS7H5008-SEP |
|
---|---|---|---|---|---|
Primary output configuration | Dual | Single | Single | Dual | |
Synchronous rectification output configuration | Dual | Single | Single | N/A | |
Duty cycle limit supported | 100%, 75%, 50% | 100%, 75% | 100%, 75% | 50% | |
Programmability of output dead-time | Yes | Yes | No, fixed at 50 ns | No | |
Leading edge blank time support | Yes | Yes | No, fixed at 50 ns | Yes | |
Target GaN FET / Si MOSFET | GaN FET or Si MOSFET | GaN FET | Si MOSFET | GaN FET or Si MOSFET | |
Topology | Buck, boost | Yes | Yes | Yes | No |
Flyback | Yes | Yes | Yes | No | |
Forward and active clamp | Yes | Yes | Yes | No | |
Push-pull | Yes | No | No | Yes | |
Half-bridge and full-bridge | Yes | No | No | Yes |
Because all flight hardware needs to understand the orbit of the satellite and its expected radiation exposure, it is not possible to select satellite devices without reviewing the mission radiation requirements.
Satellite electronics will experience three types of radiation effects while in orbit:
It’s important to validate how a component will perform when exposed to these types of radiation, especially components in the power supply. The TPS7H5001-SP device family includes TID radiation reports up to 100 krad(Si) and NDD up to 1 × 1013 neutrons/cm2, ensuring that the device passes each of the automatic test equipment test vectors post-radiation exposure that device manufacturers use to guarantee underlying data-sheet limits. For the TPS7H5001-SP SEE testing, destructive SEE testing for SEL, SEB and SEGR immunity is confirmed to a linear energy transfer (LET) equal to 75 MeV-cm2/mg, with SET and SEFI characterized to a LET equal to 75 MeV-cm2/mg.
The TPS7H5005-SEP device family includes TID radiation reports up to 50 krad(Si) and NDD up to 1 × 1013 neutrons/cm2 with destructive SEE testing for SEL, SEB and SEGR immunity is confirmed to a linear energy transfer (LET) equal to 43 MeV-cm2/mg, with SET and SEFI characterized to a LET equal to 43 MeV-cm2/mg.
Supporting the latest high-performance computing solutions in today’s smaller satellites focuses a lot of attention on the thermal design challenges of the system. The new TPS7H5001-SP and TPS7H5005-SEP PWM controller families allow designers to achieve maximum power efficiency and design flexibility. To address the ever-present radiation requirements these two families of devices also have detailed radiation reports for TID, SEE and NDD that highlight how they can support any type of orbit or mission, be it low earth orbit, medium earth orbit or a geostationary orbit.
Download the TPS7H5005-SEP flyback converter calculator.