Why Bother Turning Different Loads on and off?
STB designers usually follow standby power requirements so they can improve the system’s power efficiency. These requirements limit the amount of power that the STB can draw when it is inactive, so different
subsystems need to be off in order to draw a minimal amount of power. Some regions even have specific power requirements, such as such as Energy Star. Figure 2 shows the common STB subsystems that can be controlled to improve standby power.
Now let’s take a look at some of the subsystems you can switch on and off.
- Front end/tuner. This subsystem takes the input signal (cable or satellite) and converts the signal into video. One tuner is responsible for a single video output, so if an STB can record five shows at once, that means that there
are five different tuners dedicated to recording. Likewise, there is a tuner for the output video port and for connecting additional devices through Wi-Fi®. Switching the tuners off when they are not being used can reduce shutdown
power.
- Hard drive. A hard drive that is not recording a show or playing a previously recorded show does not need to be active. This is also the case when the STB is just outputting the cable signal.
- Wi-Fi. Wi-Fi connects additional devices to the STB such as tablets or computers, or connects smaller STBs within the same household.
Load switches can control power to each of these subsystems, and both the TPS22918 and TPS22975 can be used depending on the current load. Both are plastic devices that come with an adjustable output rise time suitable for different
capacitive loads. The TPS22918 can support loads up to 2A and the TPS22975 can support loads up to 6A.
What about Using Switches for Additional Features?
Aside from power savings, several other features require a switch:
- Power sequencing. The system on chip (SoC) or microcontroller that controls the STB has a specific power-on sequence for its different voltage rails. For optimal performance, devices like the TPS22918 or TPS22975 can turn on each
of the rails in order.
- Input protection. Voltage and current transients can occur when the 12V adapter is plugged into the STB. Placing the TPS2595 eFuse at the STB input can protect the rest of the system from hot-plug events.
- SD card. If an STB uses an SD card, the option exists to power it with 3.3V or 1.8V. Using the TPS22910A and TPS22912C load switches enables you to choose the appropriate rail.
- HDMI. The HDMI port is powered with 5V when in use, and the current needs to be limited for user protection. The TPS22945 load switch has a low current limit of 100mA.
All of these applications are modeled in the block diagram in Figure 3.
Where Can You Get Started?
The Power
Switching Reference Design for Set Top Box shows all of the different
load switches and eFuses used for each subsystem. With the added DC/DCs, the design
helps create a complete solution for STB power delivery.
With the trend in STB moving to
smaller form factors, it’s easy to see why designers are looking for more
integration in their systems. So keep your STB power design small and easy, and use
load switches and eFuses to accomplish your varying power switching needs!
Additional resources
- Only have a few minutes? Watch
some videos: