SSZTCY4 June 2023 TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TPS62874-Q1 , TPS62875-Q1 , TPS62876-Q1 , TPS62877-Q1
The electrification of vehicle systems is growing in advanced driver assistance systems (ADAS), which include vision analytics for autonomous driving, parking assistance and adaptive control functions. Smart connectivity, safety-critical software applications, and neural network processing all require enhanced computing power in real time.
Meeting these advanced needs requires a multicore processor such as the TDA4VH-Q1, which can support electronic control units (ECUs) beyond 100 A. But the design challenges associated with high power include achieving efficiency for higher current rails, controlling thermal performance and load transients at full loads, and meeting functional safety requirements.
The TPS62876-Q1 buck converter helps designers address currents beyond 30 A with a novel stackability feature that achieves the high currents necessary to power a system-on-a-chip (SoC) such as the TDA4VH-Q1. The family includes devices ranging from 15 A to 30 A, available in the same package, and Stack feature that can support to reach load current beyond 100A.
Stacking these devices not only helps power the core of next-generation ADAS SoCs, but also helps improve thermal performance by reducing thermal limitations, and increase efficiency. See Figure 1.
Stacking operates by using the daisy-chain method. The primary device controls one compensation network, one POWERGOOD pin, one ENABLE pin and one I2C interface. For optimal current sharing, you must program all devices in the stack to use same current rating, the same switching frequency and the same current level.
The primary device in the stack also sets the output voltage and controls its regulation. If there is a 47-kΩ resistor between the SYNCOUT pin and ground, the device operates as a secondary device. If the SYNCOUT pin is high impedance, the device operates as a primary device. Figure 2 shows the stack configuration implemented on a printed circuit board.
Other features in this family of buck converters include:
Functional safety is an important aspect in ADAS, especially when it comes to autonomous driving. The TPS62876-Q1 buck converter offers TI Functional Safety-Capable levels of documentation, which include:
Adding an external supervisor to your design enables you to achieve Automotive Safety Integrity Level standards.
Moving toward higher autonomy levels such as Society of Automotive Engineers Level 2 will require more computational capabilities to provide higher resolutions and quick responses in a very short time. Embedding features such as artificial intelligence technologies also increases the need for more power-hungry ADAS SoC processors. The stackability of the TPS62876-Q1 family helps you achieve core power beyond 100 A to enable a higher level of autonomous driving.