TIDUF82A August 2024 – November 2024 DRV8162 , INA241A , ISOM8710
To measure the gate voltage and the phase voltage on the switch node, the following measurements were performed. Figure 3-6 shows the test setup.
In these tests the VDC applied was 48V and the motor was set to a fixed angle with open loop vector control. The signals were measured in phase-B, including the gate voltage (CH1, in dark blue) of the low-side MOSFET, the switch node voltage (CH2, in light blue) of the phase, and the output current (CH4, in green). Both voltages are referenced to GND and the positive direction of the phase current is from the drive to the motor.
The measurements in Section 3.3.2.1, Section 3.3.2.2, and Section 3.3.2.3 show the shifts of the phase in the conditions when the current was set to both positive and negative values. All four configurations of soft switching and hard switching of the low-side MOSFET were measured.