SSZT825 January 2023 TLIN1022-Q1 , TLIN1024-Q1 , TLIN1029-Q1 , TLIN2022-Q1 , TLIN2029-Q1
Jonathan R. Claypool
When someone says “local network,” you may imagine the internet, a local area network (LAN), Wi-Fi® or Ethernet. While these technologies are robust and widespread, they require significant overhead – whether that’s wireless transceivers for Wi-Fi or protocol support to enable applications on the internet.
Highly integrated systems like automobiles need to support networks that require low overhead, so that they can be easily routed through the limited space inside the car. With electrical nodes distributed everywhere – and in great numbers – it’s also critical to reduce the cost per node.
To put this in perspective, enabling a Wi-Fi network across all control units in a car means putting a radio transmitter/receiver at every node; not only is that expensive, but antennas can be quite large on a board. Enabling Ethernet may not require radio transceivers at every node, but it does require at least four wires to implement the physical layer – four wires to send both low-speed engine control unit (ECU) data and high-speed video data. This speed/overhead trade-off led to the development of the two-wire Controller Area Network (CAN) and the one-wire Local Interconnect Network (LIN).
Designers favor CAN for its high speed (>5Mbps) and robustness to transmission faults. LIN is more like the single wire earth return (SWER) transmission lines used to bring internet to rural communities. To get online, these rural homes must connect to the main network; however, the distance and the cost of cabling to support these homes make a traditional transmission line economically unfeasible. In Figure 1 you can see a SWER power line using one wire to connect remote homes to the internet. SWER transmission lines are constructed to cover the last miles of areas that are too remote. That’s how LIN became known as the “the last mile network;” because in a car, LIN connects the remotely located nodes to the main network using a single wire.
A typical setup inside of an automobile involves a microcontroller with a CAN/LIN gateway. The CAN delivers messages to the microcontroller, which passes those messages along the LIN bus to the remote nodes. This process is depicted in Figure 2 which shows how a radar system might communicate with a seat motor via LIN. For many modules in a car, LIN is their only contact with the network. Table 1 lists the implementation differences between CAN and LIN.
![]() |
As you can see, bringing CAN to remote nodes is a serious endeavor, likely to ramp up the cost and complexity of any project. This is where LIN as the last mile network is the best solution. Integrated LIN transceivers such as TI’s TLIN1029-Q1 and TLIN2029-Q1 enable you to take full advantage of LIN’s low-cost networking in all of your 12V and 24V applications.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated