10.2.2 Design Procedure
The following procedure can be followed to design the ADC31JB68 device into most applications:
- Choose an appropriate ADC driver and analog input interface.
- Optimize the signal chain gain leading up to the ADC to make use of the full ADC dynamic range.
- Identify whether DC or AC coupling is required.
- Determine the desired analog input interface, such as a bandpass filter or a transformer.
- Use the provided input network models to design and verify the interface.
- Refer to the interface recommendations in Analog Input Considerations.
- Determine the core sampling rate of the ADC.
- Must satisfy the bandwidth requirements of the application .
- Must also provide enough margin to prevent aliasing or to accommodate the transitions bands of an anti-aliasing filter.
- Ensure the application initialization sequence properly handles ADC core calibration as described in ADC Core Calibration.
- Determine the system latency requirements.
- Total allowable latency through the ADC and JESD204B link.
- Is the system tolerant of latency variation over time or conditions or between power cycles?
- Determine the desired JESD204B link configuration as discussed in JESD204B Supported Features.
- Based on the system latency requirements, determine whether deterministic latency is required across the JESD204B link.
- Choose the number of frames per multi-frame, K.
- Choose whether scrambling is desired.
- Choose an appropriate clock generator, CLKIN interface, and SYSREF interface.
- Determine the system clock distribution scheme and the clock frequencies for the CLKIN and SYSREF inputs.
- Determine the allowable amount of sampling clock phase noise in the system and then select a CLKIN edge rate that satisfies this requirement as discussed in Internal Noise Sources.
- Choose an appropriate CLKIN interface as discussed in Driving the CLKIN+ and CLKIN– Input.
- Based on the latency requirements, determine whether SYSREF must meet setup and hold requirements relative to CLKIN.
- Choose the SYSREF signal type as discussed in SYSREF Signaling.
- Choose an appropriate SYSREF interface as discussed in Driving the SYSREF Input.
- Choose a CLKIN and SYSREF clock generator based on the above requirements. The signals must come from the same generator in many cases.
- Design the SYNCb interface as discussed in Driving the SYNCb Input.
- Choose appropriate configurations for the output serial data interface.
- Design the serial lane interface according to Output Serial-Lane Interface.
- Choose the required PCB materials, keeping in mind the desired rate of the serial lanes.
- Characterize the signal lane channels that connect the ADC serial output transmitters to the receiving device either through simulation or bench characterization.
- Optimize the VOD and DEM parameters to achieve the required signal integrity according to Voltage Swing and De-Emphasis Optimization.
- Design the SPI bus interface.
- Verify the electrical and functional compatibility of the ADC SPI with the SPI controller.
- Interface the ADC to the SPI bus according to SPI.
- Ensure that the application initialization sequence properly configures the output SDO voltage before the first read command.
- Design the power supply architecture and de-coupling.
- Choose appropriate power supply and supply filtering devices to provide stable, low-noise supplies as described in Power Supply Recommendations.
- Design the capacitive de-coupling around the ADC, also described in Power Supply Recommendations, while paying close attention to placing the capacitors as close to the device as possible.
- Time the power architecture to satisfy the power sequence requirements described in Power Supply Design.
- Ensure that the application initialization sequence satisfies the JESD204B link initialization requirements described in JESD204B Link Initialization.
- Refer to Figure 78 for an example hardware design.