JAJSE62A November 2017 – December 2021 TPS55160-Q1 , TPS55162-Q1 , TPS55165-Q1
PRODUCTION DATA
Use Equation 2 to calculate inductor peak-ripple current in the step-down, or buck, mode (Ipk_buck).
where
The maximum peak-ripple current of the inductor (Ipk) occurs when the duty cycle is at the minimum value, specifically when the input voltage (VIN) is at the maximum value which yields the value shown in Equation 4.
Substitute the values for fS, L, and Dbuck, in Equation 2 to find the peak-ripple current as shown in Equation 5.
The power dissipations can be determined by the RMS current of the inductor. Use Equation 6 to calculate the RMS current of the inductor in buck mode (Irms_buck).
Use Equation 7 to calculate the approximate power dissipation of the inductor in buck-mode (Ploss_L_buck).