JAJU648A November 2018 – April 2022 TLV3601 , TLV3601-Q1 , TLV3603 , TLV3603-Q1
To make the actual time-of-flight measurement, the TDC7201 time-to-digital converter was chosen with its fast measurement mode yielding an accuracy of 0.25 ps or 5 cm in a single-mode fiber. This mode enables high-speed measurement with a high level of accuracy that is easy to use and does not require significant processing overhead. Drive the TDC7201 input with a TLV3601 (upgrade to TLV3501) comparator that has a rise time of 0.75 ns and a delay of 2.5 ns. The laser driver pulse is set by two clock cycles of the MSP430 GPIO pin running at 12 MHz for a pulse width of 167 ns. This pulse can be shortened by using one of the PWM pins of the MSP430; however, the actual pulse duration is not critical in the measurement because the TDC7201 is set to trigger only on a rising or falling edge. Therefore, the edge rates and accuracy determine the actual measurement value.
In this measurement, the edge rate of the TLV3601 and the pulse width from the MSP430 limit the smallest and fastest pulse achievable from the design. Higher performance can be obtained by using a high-speed ADC to directly measure the output of the OPA858 and control the laser pulse with a narrower control signal. TIDA-00725 and TIDA-01187 designs describe this type of solution, but more power, a higher cost, and a more complex processing solution is required.