SBOA367B December 2019 – June 2022 TLV9001 , TLV9002 , TLV9004 , TLV9051 , TLV9052 , TLV9054 , TLV9061 , TLV9062 , TLV9064
Figure 6-1 displays an inverting amplifier circuit configuration and its equivalent model when the amplifier is placed in the shutdown mode. Notice that op amps with shutdown functionality in an inverting amplifier configuration will not block the input signal from reaching the output of the circuit when the amplifier is disabled. This is due to the path that is present from the input to the output through the feedback network while the op amp is disabled.