SBOA367B December 2019 – June 2022 TLV9001 , TLV9002 , TLV9004 , TLV9051 , TLV9052 , TLV9054 , TLV9061 , TLV9062 , TLV9064
Figure 6-3 displays a non-inverting amplifier circuit configuration and its equivalent model when the amplifier is placed in the shutdown mode. In contrast to the inverting configurations, disabling the amplifier in a non-inverting configuration ensures there is no resistive path for the input signal to reach the output node. Thus, only a smaller portion of the input signal will appear on the output when the amplifier is disabled. It is important to remember that the amplifier does have a differential input capacitance (CID) that connects the input pins and provides a path for some signal to reach the output, especially at higher frequencies.