SLAA899 December 2019 TAS2110 , TAS2555 , TAS2557 , TAS2559 , TAS2560 , TAS2562 , TAS2563 , TAS2564 , TAS2770
The inflection point sets the VBAT voltage where the AGC will begin to reduce gain below the maximum threshold. As VBAT continues to decay below this point, the AGC will track the slope setting until the minimum threshold is achieved. When the slope setting is increased the amplifier will reach the minimum threshold at higher battery voltages.