SLAA899 December 2019 TAS2110 , TAS2555 , TAS2557 , TAS2559 , TAS2560 , TAS2562 , TAS2563 , TAS2564 , TAS2770
The threshold has two settings which must be configured. The maximum threshold will determine the maximum voltage which the Class-D will output for all battery voltages. The minimum threshold will set the lowest voltage which the AGC will limit. In operation, this dictates the gain range which the AGC will utilize.