SLAAEI3 February   2024 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3519 , MSPM0L1105 , MSPM0L1106 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Relationship Between I, C and t
  5. 2Application Scenarios
  6. 3Derivation of Formulas
  7. 4Experimental Verification
    1. 4.1 Test Environment Setup
    2. 4.2 The Result of Experiment
  8. 5Notes

Application Scenarios

  • With unstable power supply, the capacitor can be used as a backup power supply to support the MCU to operate for a certain period of time until the power supply is restored, or to provide a certain amount of time to save the MCU's data.
  • In the printer cartridge, the three-wire system cannot meet the MCU communication needs, as UART need two wires, VCC one and Ground one. Here we can multiplex the VCC end with the TXD of the UART. While TXD is high, it can charge capacitor as well as supply power for MCU. And as TXD goes to LOW, a diode can separate the VCC terminal of TXD from the MCU, and rely on the capacitor to power the MCU.