SLAAEI3 February 2024 MSPM0C1103 , MSPM0C1104 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0L1105 , MSPM0L1106 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2228 , MSPM0L2228-Q1
The Figure 4-3 is the experimental result of operating current of MCU run in run0 mode. Both EnergyTrace and direct measurement are all show the run0 current is around 1.5mA.
The power supply of MCU2 was monitored using a logic analyzer and the results are shown in the figure. Channel 1 identifies the GPIO port, and when set to low, MCU1's GPIO is in a high-impedance condition, and MCU2 is powered only by capacitors. Channel 2 is the voltage on both sides of the capacitor, which is the supply voltage of the MCU. As can be seen from the figure, when the voltage drops from 3.3 V to 1.61 V, the duration is about 2.66ms, which is close to the theoretical calculation of 2.56 ms.
Table 4-1 shows a table summary of the working time of different capacitors in each operating mode.
Capacitors | STOP0 I=0.32mA | RUN0 I=1.5mA | |||
---|---|---|---|---|---|
Type | Capacitance | Measurement Time | Calculation Time | Measurement Time | Calculation Time |
Tantalum capacitors TAJA225K010RNJ |
2.2μF | 12.01ms | 11.55ms | 2.66ms | 2.56ms |
Tantalum capacitors TAJA475K010RNJ |
4.7μF | 23.29ms | 24.68ms | 5.10ms | 5.48ms |
Tantalum capacitors TAJA106K010RNJ |
10μF | 56.72ms | 56.00ms | 12.33ms | 11.67ms |
Electrolytic capacitors ASLI-D37 |
10μF | 53.79ms | 56.00ms | 11.35ms | 11.67ms |
Electrolytic capacitors ASLI-E13 |
40μF | 278.95ms | 263.2ms | 57.59ms | 54.33ms |
Ceramic capacitors GRM21BR61A |
2μF | 12.15ms | 11.2ms | 12.15ms | 11.20ms |
Ceramic capacitors GRM21BR61A |
4.3μF | 22.76ms | 22.58ms | 4.88ms | 5.02ms |
Ceramic capacitors GRM21BR61A |
6.3μF | 34.08ms | 33.08ms | 7.30ms | 7.35ms |
As can be seen from the table, the theoretical calculated value is basically consistent with the actual measurement. The reasons for some errors can be: capacitance error value; There is a leakage condition in the meter pen; Cable resistance, energy dissipation, etc. But, the error is within a reasonable range.