SLAU367P October 2012 – April 2020 MSP430FR5041 , MSP430FR5043 , MSP430FR50431 , MSP430FR5847 , MSP430FR58471 , MSP430FR5848 , MSP430FR5849 , MSP430FR5857 , MSP430FR5858 , MSP430FR5859 , MSP430FR5867 , MSP430FR58671 , MSP430FR5868 , MSP430FR5869 , MSP430FR5870 , MSP430FR5872 , MSP430FR58721 , MSP430FR5887 , MSP430FR5888 , MSP430FR5889 , MSP430FR58891 , MSP430FR5922 , MSP430FR59221 , MSP430FR5947 , MSP430FR59471 , MSP430FR5948 , MSP430FR5949 , MSP430FR5957 , MSP430FR5958 , MSP430FR5959 , MSP430FR5962 , MSP430FR5964 , MSP430FR5967 , MSP430FR5968 , MSP430FR5969 , MSP430FR5969-SP , MSP430FR59691 , MSP430FR5970 , MSP430FR5972 , MSP430FR59721 , MSP430FR5986 , MSP430FR5987 , MSP430FR5988 , MSP430FR5989 , MSP430FR5989-EP , MSP430FR59891 , MSP430FR5992 , MSP430FR5994 , MSP430FR59941 , MSP430FR6005 , MSP430FR6007 , MSP430FR6035 , MSP430FR6037 , MSP430FR60371 , MSP430FR6041 , MSP430FR6043 , MSP430FR60431 , MSP430FR6045 , MSP430FR6047 , MSP430FR60471 , MSP430FR6820 , MSP430FR6822 , MSP430FR68221 , MSP430FR6870 , MSP430FR6872 , MSP430FR68721 , MSP430FR6877 , MSP430FR6879 , MSP430FR68791 , MSP430FR6887 , MSP430FR6888 , MSP430FR6889 , MSP430FR68891 , MSP430FR6920 , MSP430FR6922 , MSP430FR69221 , MSP430FR6927 , MSP430FR69271 , MSP430FR6928 , MSP430FR6970 , MSP430FR6972 , MSP430FR69721 , MSP430FR6977 , MSP430FR6979 , MSP430FR69791 , MSP430FR6987 , MSP430FR6988 , MSP430FR6989 , MSP430FR69891
The PMM registers are listed in Table 2-1. The base address of the PMM module can be found in the device-specific data sheet. The address offset of each PMM register is given in Table 2-1.
The password defined in the PMMCTL0 register controls access to all PMM registers except PM5CTL0. PM5CTL0 can be accessed without a password. After the correct password is written, the write access is enabled (this includes byte access to the PMMCTL0 lower byte). The write access is disabled by writing a wrong password in byte mode to the PMMCTL0 upper byte. Word accesses to PMMCTL0 with a wrong password triggers a PUC. A write access to a register other than PMMCTL0 while write access is not enabled causes a PUC.
NOTE
All registers have word or byte register access. For a generic register ANYREG, the suffix "_L" (ANYREG_L) refers to the lower byte of the register (bits 0 through 7). The suffix "_H" (ANYREG_H) refers to the upper byte of the register (bits 8 through 15).
Offset | Acronym | Register Name | Type | Access | Reset | Section |
---|---|---|---|---|---|---|
00h | PMMCTL0 | PMM control register 0 | Read/write | Word | 9640h | Section 2.3.1 |
00h | PMMCTL0_L | Read/write | Byte | 40h | ||
01h | PMMCTL0_H | Read/write | Byte | 96h | ||
02h | PMMCTL1 | PMM control register 1 | Read/write(1) | Word | 9600h | Section 2.3.2 |
02h | PMMCTL1_L | Read(1) | Byte | 00h | ||
03h | PMMCTL1_H | Read(1) | Byte | 96h | ||
0Ah | PMMIFG | PMM interrupt flag register | Read/write | Word | 0000h | Section 2.3.3 |
0Ah | PMMIFG_L | Read/write | Byte | 00h | ||
0Bh | PMMIFG_H | Read/write | Byte | 00h | ||
10h | PM5CTL0 | Power mode 5 control register 0 | Read/write | Word | 0001h | Section 2.3.4 |
10h | PM5CTL0_L | Read/write | Byte | 01h | ||
11h | PM5CTL0_H | Read/write | Byte | 00h |