SLLA472A March 2020 – February 2022 ISO5852S , ISO5852S-EP , ISO5852S-Q1 , LM5106
Boards were designed and made for BJT-based and MOSFET-based current-boosted gate drivers and their comparative performance was evaluated. The MOSFET based saturated drive was found to be able to give more drive current and was relatively cooler while driving similar loads. The BJT drive was simpler with the ability to extend the protection features offered by the gate driver IC used. The BJT drive also provides a much higher level of integration.