SLLA486A May 2020 – May 2021 ISO1042 , ISO1042-Q1 , ISO1044 , ISO1050 , ISOW1044
Most isolated or non-isolated CAN transceivers have a protection feature called Dominant-Timeout (DTO). This feature disables the transmitter of a device if it holds the bus dominant for a time greater than DTO. This feature is useful in case of a software failure or a hardware failure that makes TXD low continuously. The CAN protocol does not allow transmission of more than 5 bits of same state in a row due to bit stuffing rules except in error condition. So in an error scenario, 5 dominant bits followed by 6 consecutive dominant bits of error frame needs to be transmitted. Hence, 11*bit time of one dominant bit <= DTO time. This decides minimum data rate (or maximum one bit dominant time period).
Though ISO1042, ISO1044, and ISOW1044 are able to support a maximum 5 Mbps data rate, the actual maximum achievable in a network is dependent on maximum cable length (for example, distance between farthest nodes), type of cable (which will decide signal speed in the interconnect medium), and total capacitance that exists across the CAN bus due to cable, individual nodes, PCB traces, connectors, and so forth. Bitwise arbitration is the key to CAN protocol. This means during arbitration phase of CAN packet, a bit sent by a transmitter needs to reach the farthest receiver and back to the transmitter which monitors via RXD for it to move to the subsequent bit in the CAN-ID part of a data packet. So the fastest bit time in arbitration phase has to be more than the loop delay of a transmitter node + 2*prop delay of cable (typically 5 ns/meter of CAT5e cable). This indicates there is an inverse relationship between maximum data rate in arbitration period and maximum communication distance. The maximum data rate during data-phase of CAN packet would be limited by the bit timing distortion introduced by the transceiver and by the controller's sampling point margin. Overall capacitance seen on the bus also impacts timing as dominant to recessive edge transitions may be elongated if a higher capacitance is seen on the bus.